MATHLIB User Guide
MATHLIB_log.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_log (size_t length, T *pSrc, T *pDst)
 Performs the elementwise log of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise log of the input vector. More...
 
MATHLIB_STATUS MATHLIB_log_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_log. Function accepts float pointers. More...