MATHLIB User Guide
MATHLIB_log10.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_log10 (size_t length, T *pSrc, T *pDst)
 Performs the elementwise log base 10 of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise log base 10 of the input vector. More...
 
MATHLIB_STATUS MATHLIB_log10_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_log10. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_log10_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_log10. Function accepts double pointers. More...