![]() |
TI J721E Imaging User Guide
|
Data Fields | |
| uint32_t | header |
| char | cmd [NETWORK_CTRL_CMD_STRLEN_MAX] |
| uint32_t | returnValue |
| uint32_t | flags |
| uint32_t | prmSize |
| uint32_t NetworkCtrl_CmdHeader::header |
Header magic number NETWORK_CTRL_HEADER
| char NetworkCtrl_CmdHeader::cmd[NETWORK_CTRL_CMD_STRLEN_MAX] |
Command, specified as a string of char's
| uint32_t NetworkCtrl_CmdHeader::returnValue |
Return value that is set by the command handler
| uint32_t NetworkCtrl_CmdHeader::flags |
command specified flags, see NETWORK_CTRL_FLAG_*
| uint32_t NetworkCtrl_CmdHeader::prmSize |
Size of input parameters in units of bytes. Can be 0 if no parameters need to sent for a command