TI J721E Imaging User Guide
itt_ctrl_handle_sensor.c File Reference

Macros

#define I2C_BUS   5
 
#define SLAVE_REG   0x4a
 

Functions

int i2c16BitRegRead (uint16_t regAddr, uint8_t *regData)
 
int i2c16BitRegWrite (uint16_t regAddr, uint8_t regData)
 
void itt_ctrl_cmdHandlerIssReadSensorReg (char *cmd, uint32_t prmSize)
 Handler for command "iss_read_sensor_reg". Function callback passed to network_api utils. Must comply with the syntax of NetworkCtrl_Handler Inputs. More...
 
void itt_ctrl_cmdHandlerIssWriteSensorReg (char *cmd, uint32_t prmSize)
 Handler for command "iss_write_sensor_reg". Function callback passed to network_api utils. Must comply with the syntax of NetworkCtrl_Handler Inputs. More...
 
int i2cInit ()
 

Variables

int file_g = -1
 
static uint8_t cmd_param_sensor_ctrl [CMD_PARAM_SIZE]
 
uint8_t gEdgeAI
 

Macro Definition Documentation

◆ I2C_BUS

#define I2C_BUS   5

◆ SLAVE_REG

#define SLAVE_REG   0x4a

Function Documentation

◆ i2c16BitRegRead()

int i2c16BitRegRead ( uint16_t  regAddr,
uint8_t *  regData 
)

◆ i2c16BitRegWrite()

int i2c16BitRegWrite ( uint16_t  regAddr,
uint8_t  regData 
)

◆ i2cInit()

int i2cInit ( )

Variable Documentation

◆ file_g

int file_g = -1

◆ cmd_param_sensor_ctrl

uint8_t cmd_param_sensor_ctrl[CMD_PARAM_SIZE]
static

◆ gEdgeAI

uint8_t gEdgeAI