DSPLIB User Guide
DSPLIB_qrd_solver_PrivArgs Struct Reference

Detailed Description

Structure that is reserved for internal use by the kernel.

Definition at line 195 of file DSPLIB_qrd_solver_priv.h.

Data Fields

pFxnDSPLIB_qrd_solver_exec execute
 Function pointer to point to the right execution variant between DSPLIB_qrd_solver_exec_cn and DSPLIB_qrd_solver_exec_ci.
More...
 
uint32_t widthR
 Size of input buffer for different batches DSPLIB_qrd_solver_init that will be retrieved and used by DSPLIB_qrd_solver_exec
More...
 
uint32_t heightR
 Height of input data matrix
More...
 
int32_t strideQ
 Stride between rows of Q output data matrix
More...
 
int32_t strideR
 Stride between rows of R output data matrix
More...
 
DSPLIB_matTrans_PrivArgs pMatTransKerPrivArgs
 Privargs for the matTrans kernel. More...
 
uint8_t bufPblock [DSPLIB_QRD_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE]
 Buffer to save SE & SA configuration parameters
More...
 

Field Documentation

◆ execute

pFxnDSPLIB_qrd_solver_exec DSPLIB_qrd_solver_PrivArgs::execute

Function pointer to point to the right execution variant between DSPLIB_qrd_solver_exec_cn and DSPLIB_qrd_solver_exec_ci.

Definition at line 199 of file DSPLIB_qrd_solver_priv.h.

◆ widthR

uint32_t DSPLIB_qrd_solver_PrivArgs::widthR

Size of input buffer for different batches DSPLIB_qrd_solver_init that will be retrieved and used by DSPLIB_qrd_solver_exec

Width of input data matrix

Definition at line 204 of file DSPLIB_qrd_solver_priv.h.

◆ heightR

uint32_t DSPLIB_qrd_solver_PrivArgs::heightR

Height of input data matrix

Definition at line 206 of file DSPLIB_qrd_solver_priv.h.

◆ strideQ

int32_t DSPLIB_qrd_solver_PrivArgs::strideQ

Stride between rows of Q output data matrix

Definition at line 208 of file DSPLIB_qrd_solver_priv.h.

◆ strideR

int32_t DSPLIB_qrd_solver_PrivArgs::strideR

Stride between rows of R output data matrix

Definition at line 210 of file DSPLIB_qrd_solver_priv.h.

◆ pMatTransKerPrivArgs

DSPLIB_matTrans_PrivArgs DSPLIB_qrd_solver_PrivArgs::pMatTransKerPrivArgs

Privargs for the matTrans kernel.

Definition at line 212 of file DSPLIB_qrd_solver_priv.h.

◆ bufPblock

uint8_t DSPLIB_qrd_solver_PrivArgs::bufPblock[DSPLIB_QRD_SOLVER_IXX_IXX_OXX_PBLOCK_SIZE]

Buffer to save SE & SA configuration parameters

Definition at line 214 of file DSPLIB_qrd_solver_priv.h.