DSPLIB User Guide
DSPLIB_negate_PrivArgs Struct Reference

Detailed Description

Structure that is reserved for internal use by the kernel.

Definition at line 151 of file DSPLIB_negate_priv.h.

Data Fields

pFxnDSPLIB_negate_exec execute
 Function pointer to point to the right execution variant between DSPLIB_negate_exec_cn and DSPLIB_negate_exec_ci.
More...
 
int32_t blockSize
 Size of input buffer for different batches DSPLIB_negate_init that will be retrieved and used by DSPLIB_negate_exec
More...
 
uint8_t bufPblock [DSPLIB_NEGATE_IXX_IXX_OXX_PBLOCK_SIZE]
 

Field Documentation

◆ execute

pFxnDSPLIB_negate_exec DSPLIB_negate_PrivArgs::execute

Function pointer to point to the right execution variant between DSPLIB_negate_exec_cn and DSPLIB_negate_exec_ci.

Definition at line 155 of file DSPLIB_negate_priv.h.

◆ blockSize

int32_t DSPLIB_negate_PrivArgs::blockSize

Size of input buffer for different batches DSPLIB_negate_init that will be retrieved and used by DSPLIB_negate_exec

Definition at line 159 of file DSPLIB_negate_priv.h.

◆ bufPblock

uint8_t DSPLIB_negate_PrivArgs::bufPblock[DSPLIB_NEGATE_IXX_IXX_OXX_PBLOCK_SIZE]

Definition at line 161 of file DSPLIB_negate_priv.h.