DSPLIB User Guide
DSPLIB_minerror_InitArgs Struct Reference

Detailed Description

Structure containing the parameters to initialize the kernel.

Definition at line 108 of file DSPLIB_minerror.h.

Data Fields

int8_t funcStyle
 Variant of the function refer to DSPLIB_FUNCTION_STYLE
More...
 
uint32_t vecInSize
 Size of input data
More...
 
uint32_t errCoefsSize
 Size of error coefficients vector
More...
 
uint32_t strideIn
 

Field Documentation

◆ funcStyle

int8_t DSPLIB_minerror_InitArgs::funcStyle

Variant of the function refer to DSPLIB_FUNCTION_STYLE

Definition at line 110 of file DSPLIB_minerror.h.

◆ vecInSize

uint32_t DSPLIB_minerror_InitArgs::vecInSize

Size of input data

Definition at line 112 of file DSPLIB_minerror.h.

◆ errCoefsSize

uint32_t DSPLIB_minerror_InitArgs::errCoefsSize

Size of error coefficients vector

Definition at line 114 of file DSPLIB_minerror.h.

◆ strideIn

uint32_t DSPLIB_minerror_InitArgs::strideIn

Definition at line 115 of file DSPLIB_minerror.h.