![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 132 of file DSPLIB_cholesky_inplace_priv.h.
Data Fields | |
| pFxnDSPLIB_cholesky_inplace_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_cholesky_inplace_exec_cn and DSPLIB_cholesky_inplace_exec_ci. More... | |
| int32_t | order |
| Order of input buffer for different batches DSPLIB_cholesky_inplace_init that will be retrieved and used by DSPLIB_cholesky_inplace_exec More... | |
| int32_t | stride |
| int32_t | enableTest |
| int32_t | shiftForVecLenDiv |
| uint8_t | bufPblock [DSPLIB_CHOLESKY_INPLACE_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_cholesky_inplace_exec DSPLIB_cholesky_inplace_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_cholesky_inplace_exec_cn and DSPLIB_cholesky_inplace_exec_ci.
Definition at line 136 of file DSPLIB_cholesky_inplace_priv.h.
| int32_t DSPLIB_cholesky_inplace_PrivArgs::order |
Order of input buffer for different batches DSPLIB_cholesky_inplace_init that will be retrieved and used by DSPLIB_cholesky_inplace_exec
Definition at line 140 of file DSPLIB_cholesky_inplace_priv.h.
| int32_t DSPLIB_cholesky_inplace_PrivArgs::stride |
Definition at line 141 of file DSPLIB_cholesky_inplace_priv.h.
| int32_t DSPLIB_cholesky_inplace_PrivArgs::enableTest |
Definition at line 142 of file DSPLIB_cholesky_inplace_priv.h.
| int32_t DSPLIB_cholesky_inplace_PrivArgs::shiftForVecLenDiv |
Definition at line 143 of file DSPLIB_cholesky_inplace_priv.h.
| uint8_t DSPLIB_cholesky_inplace_PrivArgs::bufPblock[DSPLIB_CHOLESKY_INPLACE_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 144 of file DSPLIB_cholesky_inplace_priv.h.