81 #ifndef DSPLIB_W_VEC_IXX_IXX_OXX_H_
82 #define DSPLIB_W_VEC_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
209 const void *restrict pIn1,
210 const void *restrict pIn2,
211 const void *restrict pM,
212 const void *restrict pOut);
248 void *restrict pOut);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
int32_t DSPLIB_w_vec_getHandleSize(DSPLIB_w_vec_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_w_vec_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_w_vec_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_w_vec_exec function is called. This function takes c...
DSPLIB_STATUS DSPLIB_w_vec_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_w_vec_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_w_vec_init function....
DSPLIB_STATUS DSPLIB_w_vec_exec(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_w_vec_weightStyle
Enumeration for w_vec flag pertaining to scalar or vector input weight.
DSPLIB_STATUS DSPLIB_w_vec_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn1, const void *restrict pIn2, const void *restrict pM, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_w_vec_exec function....
@ DSPLIB_SCALAR
Input Weight is a Scalar.
@ DSPLIB_VECTOR
Input Weight is a Vector.
A structure for a 1 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
DSPLIB_w_vec_weightStyle weightStyle
Weight Input Style
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
uint32_t dataSize
Size of input data