Go to the source code of this file.
◆ DSPLIB_q15tofl_init_cn()
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_q15tofl_init.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 31 of file DSPLIB_q15tofl_cn.cpp.
◆ DSPLIB_q15tofl_exec_cn()
template<typename dataTypeOut >
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_q15tofl_exec.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 41 of file DSPLIB_q15tofl_cn.cpp.
◆ DSPLIB_q15tofl_exec_cn< float >()
◆ DSPLIB_q15tofl_exec_cn< double >()