21 #ifndef DSPLIB_MININDEX_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_MININDEX_IXX_IXX_OXX_PRIV_H_
24 #include "../common/DSPLIB_utility.h"
37 #define SE_PARAM_BASE (0x0000)
38 #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE)
39 #define SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE)
46 #define DSPLIB_MININDEX_IXX_IXX_OXX_PBLOCK_SIZE (1 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
81 template <
typename dataType>
111 template <
typename T,
typename TIndex>
128 template <
typename dataType>
146 template <
typename T,
typename TIndex>
struct metadata {
148 typedef typename c7x::make_full_vector<T>::type
vec;
149 typedef typename c7x::make_full_vector<TIndex>::type
index_vec;
metadata< T, TIndex > DSPLIB_minIndex_loopLogic(size_t length, void *pSrc)
This function is the kernel loop helper function for the optimized implementation of the kernel....
#define DSPLIB_MININDEX_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_minIndex_PrivArgs structure.
DSPLIB_STATUS DSPLIB_minIndex_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS(* pFxnDSPLIB_minIndex_exec)(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_minIndex_exec_ci and DSPLI...
DSPLIB_STATUS DSPLIB_minIndex_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_minIndex_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_minIndex_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 1 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
int32_t blockSize
Size of input buffer for different batches DSPLIB_minIndex_init that will be retrieved and used by DS...
pFxnDSPLIB_minIndex_exec execute
Function pointer to point to the right execution variant between DSPLIB_minIndex_exec_cn and DSPLIB_m...