81 #ifndef DSPLIB_MATMUL_FIXED_IXX_IXX_OXX_H_
82 #define DSPLIB_MATMUL_FIXED_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
201 const void *restrict pIn0,
202 const void *restrict pIn1,
203 const void *restrict pOut);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
int32_t DSPLIB_matMul_fixed_getHandleSize(DSPLIB_matMul_fixed_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_matMul_fixed_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn0, const void *restrict pIn1, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_exec function....
DSPLIB_STATUS DSPLIB_matMul_fixed_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn0, DSPLIB_bufParams2D_t *bufParamsIn1, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_fixed_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_matMul_fixed_exec function is called....
DSPLIB_STATUS DSPLIB_matMul_fixed_exec(DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_matMul_fixed_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn0, const DSPLIB_bufParams2D_t *bufParamsIn1, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_fixed_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_init function....
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE