Go to the source code of this file.
|
| DSPLIB_STATUS | DSPLIB_fir_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_fir_InitArgs *pKerInitArgs) |
| | This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_fir_init. More...
|
| |
| template<typename dataType , typename accumulateType > |
| DSPLIB_STATUS | DSPLIB_fir_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| | This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_fir_exec. More...
|
| |
| template DSPLIB_STATUS | DSPLIB_fir_exec_cn< int16_t, int64_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_fir_exec_cn< int32_t, DSPLIB_int128_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_fir_exec_cn< int8_t, int32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| |
| template DSPLIB_STATUS | DSPLIB_fir_exec_cn< float, int32_t > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut) |
| |
◆ DSPLIB_fir_init_cn()
This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_fir_init.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 31 of file DSPLIB_fir_cn.cpp.
◆ DSPLIB_fir_exec_cn()
template<typename dataType , typename accumulateType >
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_fir_exec.
- Parameters
-
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the filter data |
| [out] | pOut | : Pointer to buffer holding the output data |
- Returns
- Status value indicating success or failure. Refer to DSPLIB_STATUS.
Definition at line 43 of file DSPLIB_fir_cn.cpp.
◆ DSPLIB_fir_exec_cn< int16_t, int64_t >()
◆ DSPLIB_fir_exec_cn< int32_t, DSPLIB_int128_t >()
◆ DSPLIB_fir_exec_cn< int8_t, int32_t >()
◆ DSPLIB_fir_exec_cn< float, int32_t >()