![]() |
DSPLIB User Guide
|
Definition in file DSPLIB_cholesky.cpp.
Go to the source code of this file.
Functions | |
| int32_t | DSPLIB_cholesky_getHandleSize (DSPLIB_cholesky_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_cholesky_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_cholesky_init function. This function is called with the same parameters as the DSPLIB_cholesky_init, and this function must be called before the DSPLIB_cholesky_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_cholesky_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_cholesky_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_cholesky_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pInA, const void *restrict pOutU, const void *restrict pMul) |
| This function checks the validity of the parameters passed to DSPLIB_cholesky_exec function. This function is called with the same parameters as the DSPLIB_cholesky_init, and this function must be called before the DSPLIB_cholesky_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_cholesky_exec (DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict pMul) |
| This function is the main kernel compute function. More... | |