Go to the source code of this file.
|
| int32_t | DSPLIB_bexp_getHandleSize (DSPLIB_bexp_InitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_bexp_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_bexp_InitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_bexp_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources, streaming engine in this case. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_bexp_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_bexp_InitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_bexp_init function. This function is called with the same parameters as the DSPLIB_bexp_init, and this function must be called before the DSPLIB_bexp_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_bexp_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut) |
| | This function checks the validity of the parameters passed to DSPLIB_bexp_exec function. This function is called with the same parameters as the DSPLIB_bexp_exec, and this function must be called before the DSPLIB_bexp_exec is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_bexp_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| | This function is the main kernel compute function. More...
|
| |