21 #ifndef DSPLIB_ADD_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_ADD_IXX_IXX_OXX_PRIV_H_
24 #include "../common/DSPLIB_utility.h"
39 #define DSPLIB_ADD_IXX_IXX_OXX_PBLOCK_SIZE (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
78 template <
typename dataType>
109 template <
typename dataType>
132 template <
typename dataType>
DSPLIB_STATUS(* pFxnDSPLIB_add_exec)(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_add_exec_ci and DSPLIB_add...
DSPLIB_STATUS DSPLIB_add_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_add_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_add_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
#define DSPLIB_ADD_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_add_PrivArgs structure.
DSPLIB_STATUS DSPLIB_add_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut)
This function is the initialization function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_add_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_add_exec execute
Function pointer to point to the right execution variant between DSPLIB_add_exec_cn and DSPLIB_add_ex...
int32_t blockSize
Size of input buffer for different batches DSPLIB_add_init that will be retrieved and used by DSPLIB_...
A structure for a 1 dimensional buffer descriptor.
A structure for a 2 dimensional buffer descriptor.