TI Deep Learning Product User Guide
sTIDL_DataParams_t Struct Reference

Detailed Description

This structure define the parameters of data or kernel buffer used by TIDL layers (In,Out)

Data Fields

int32_t dataId
 
int32_t elementType
 
int32_t numDim
 
int32_t dataQ
 
int32_t minValue
 
int32_t maxValue
 
float32_tidl minTensorValue
 
float32_tidl maxTensorValue
 
float32_tidl tensorScale
 
int32_t tensorZeroPoint
 
int32_t tensorType
 
int32_t padW
 
int32_t padH
 
int32_t batchPadW
 
int32_t batchPadH
 
int32_t numBatchW
 
int32_t numBatchH
 
int32_t roundBits
 
int32_t pitch [TIDL_DIM_MAX-1U]
 
int32_t dimValues [TIDL_DIM_MAX]
 

Field Documentation

◆ dataId

int32_t sTIDL_DataParams_t::dataId

Unique Data ID for the tensor holding feature vector

◆ elementType

int32_t sTIDL_DataParams_t::elementType

Element type of the feature vector as defined in eTIDL_ElementType

◆ numDim

int32_t sTIDL_DataParams_t::numDim

Number of dimensions supported by the tensor

◆ dataQ

int32_t sTIDL_DataParams_t::dataQ

Q factor used for fixed point : NOT used now

◆ minValue

int32_t sTIDL_DataParams_t::minValue

Minimum value of Accumulator in fixed point : NOT used now

◆ maxValue

int32_t sTIDL_DataParams_t::maxValue

Maximum value of Accumulator in fixed point : NOT used now

◆ minTensorValue

float32_tidl sTIDL_DataParams_t::minTensorValue

Minimum value of Accumulator in floating point

◆ maxTensorValue

float32_tidl sTIDL_DataParams_t::maxTensorValue

Maximum value of Accumulator in floating point

◆ tensorScale

float32_tidl sTIDL_DataParams_t::tensorScale

Scale value applied on the tensor for final fixed point

◆ tensorZeroPoint

int32_t sTIDL_DataParams_t::tensorZeroPoint

Zero point value used in conjunction with the tensor scale to quantize/dequantize tensors

◆ tensorType

int32_t sTIDL_DataParams_t::tensorType

Is the tensor symmetric (zero point = 0) or asymmetric

◆ padW

int32_t sTIDL_DataParams_t::padW

Horizontal Padding

◆ padH

int32_t sTIDL_DataParams_t::padH

Vertical Padding

◆ batchPadW

int32_t sTIDL_DataParams_t::batchPadW

Padding between horizontal Batches in stitched image

◆ batchPadH

int32_t sTIDL_DataParams_t::batchPadH

Padding between vertical Batches in the stitched image

◆ numBatchW

int32_t sTIDL_DataParams_t::numBatchW

Number of Batches stitched in the width direction for batch processing

◆ numBatchH

int32_t sTIDL_DataParams_t::numBatchH

Number of Batches stitched in the height direction for batch processing

◆ roundBits

int32_t sTIDL_DataParams_t::roundBits

Rounding bit used while converting to small bit depth (8 or 16 bit)

◆ pitch

int32_t sTIDL_DataParams_t::pitch[TIDL_DIM_MAX-1U]

Pitch for each dimension as defined by eTIDL_PitchDimIndex

◆ dimValues

int32_t sTIDL_DataParams_t::dimValues[TIDL_DIM_MAX]

Values of dimensions as defined by eTIDL_DataDimIndex