This structure contains all the parameters which are given as an input to OD algorithm at frame level.
More...
#include <tiadalg_structure_from_motion.h>
This structure contains all the parameters which are given as an input to OD algorithm at frame level.
- Parameters
-
| iVisionInArgs | Common InArgs for all ivison based modules |
| flowConfThr | Optical flow confidence threshold |
| flowInvalidPadX | Number of pixels to be ignored in optical buffer in x direction |
| flowInvalidPadY | Number of pixels to be ignored in optical buffer in y direction |
| camExtPrm | : Camera Extrinsic Parameters. Format of camera extrinsic parameters is [ r00 r01 r02 t0 r10 r11 r12 t1 r20 r21 r22 t2], where rij are the rotation parameter, and ti are the translation parameter. If this pointer is provided as NULL, then these parameters are computed internally. |
| fMatCalcMethod | This controls how Fundamental Matrix is estimated/calculated. There is possibility of estimating Fundamental matrix using feature point correspondence between two frames, whereas there could be another method to calculate using rotation and translation parameters provided. Refer for various supported values and default values. |
| fMatrixPrunEn | Control to enable or disable Fundamental matrix based pruning of the input tracks. User should set this as '1' to enable this pruning. |
| fMatrixInTh | Inlier threshold used in Fundamental matrix based pruning. |
| maxRansacItr | Maximum number of RANSAC iteration in F matrix iteration. Its Supported value is [0, 200]. User should set default value for this as 90. When value zero is set then algorithm does optimal number of iterations. |
| maxTriangItr | Maximum number of iteration in triangulation. Supported value for this is [1,10]. User should set default value which is 4. |
| pointPruneAngle | Angle threshold used for angle based pruning. Supported Values is [0.0 10.0] |
| staticFrmTh | Threshold to determine wheather current frame is static or not. Norm of the current frame camera translation with respect to previous frame should be less than this threshold to flag current frame as static frame. Not used in current version. |
| reset | resets the algorithm from this frame onward. Past tracks are ignored and it will get built up again from this frame onward. |
| reserved0 | Reserved 32-bit field. Must be set to 0 for normal operation. |
| reserved1 | Reserved 32-bit field. Must be set to 0 for normal operation. |
◆ iVisionInArgs
| IVISION_InArgs SFM_TI_InArgs::iVisionInArgs |
◆ flowConfThr
| int32_t SFM_TI_InArgs::flowConfThr |
◆ flowInvalidPadX
| int32_t SFM_TI_InArgs::flowInvalidPadX |
◆ flowInvalidPadY
| int32_t SFM_TI_InArgs::flowInvalidPadY |
◆ camExtPrm
◆ fMatrixCalcMethod
| uint32_t SFM_TI_InArgs::fMatrixCalcMethod |
◆ fMatrixPrunEn
| uint32_t SFM_TI_InArgs::fMatrixPrunEn |
◆ fMatrixInTh
| uint32_t SFM_TI_InArgs::fMatrixInTh |
◆ maxRansacItr
| uint32_t SFM_TI_InArgs::maxRansacItr |
◆ maxTriangItr
| uint32_t SFM_TI_InArgs::maxTriangItr |
◆ pointPruneAngle
| float SFM_TI_InArgs::pointPruneAngle |
◆ staticFrmTh
| float SFM_TI_InArgs::staticFrmTh |
◆ reset
| int32_t SFM_TI_InArgs::reset |
◆ reserved0
| uint32_t SFM_TI_InArgs::reserved0 |
◆ reserved1
| uint32_t SFM_TI_InArgs::reserved1 |
The documentation for this struct was generated from the following file: