![]() |
PDK API Guide for J742S2
|
Event module for the RTOS Porting Interface.
============================================================================
Go to the source code of this file.
Status codes for EventP APIs | |
| #define | EventP_OK ((int32_t) 0) |
| #define | EventP_FAILURE ((int32_t) (-1)) |
| typedef int32_t | EventP_Status |
| Status codes for EventP APIs. More... | |
Event wait modes for EventP_wait API | |
| #define | EventP_WaitMode_ANY ( (uint8_t) 0U) |
| #define | EventP_WaitMode_ALL ( (uint8_t) 1U) |
| typedef uint8_t | EventP_WaitMode |
| This enumerator defines the Event wait modes. More... | |
Data Structures | |
| struct | EventP_Params |
| Basic EventP Parameters. More... | |
Macros | |
| #define | EventP_WAIT_FOREVER (~((uint32_t)0U)) |
| Wait forever define. More... | |
| #define | EventP_NO_WAIT ((uint32_t)0U) |
| No wait define. More... | |
Event ID definitions | |
Pre-defined Event Ids. EventP_Ids are provided to simplify the specification of mask argument to EventP_wait(). Since each EventP_Id is a bitmask composed of only a single bit, a group of EventP_Ids within a Mask can be indicated by simply adding them together. | |
| #define | EventP_ID_NONE 0x0U |
| Event ID NONE. More... | |
| #define | EventP_ID_00 0x1U |
| Event ID 0. More... | |
| #define | EventP_ID_01 0x2U |
| Event ID 1. More... | |
| #define | EventP_ID_02 0x4U |
| Event ID 2. More... | |
| #define | EventP_ID_03 0x8U |
| Event ID 3. More... | |
| #define | EventP_ID_04 0x10U |
| Event ID 4. More... | |
| #define | EventP_ID_05 0x20U |
| Event ID 5. More... | |
| #define | EventP_ID_06 0x40U |
| Event ID 6. More... | |
| #define | EventP_ID_07 0x80U |
| Event ID 7. More... | |
| #define | EventP_ID_08 0x100U |
| Event ID 8. More... | |
| #define | EventP_ID_09 0x200U |
| Event ID 9. More... | |
| #define | EventP_ID_10 0x400U |
| Event ID 10. More... | |
| #define | EventP_ID_11 0x800U |
| Event ID 11. More... | |
| #define | EventP_ID_12 0x1000U |
| Event ID 12. More... | |
| #define | EventP_ID_13 0x2000U |
| Event ID 13. More... | |
| #define | EventP_ID_14 0x4000U |
| Event ID 14. More... | |
| #define | EventP_ID_15 0x8000U |
| Event ID 15. More... | |
| #define | EventP_ID_16 0x10000U |
| Event ID 16. More... | |
| #define | EventP_ID_17 0x20000U |
| Event ID 17. More... | |
| #define | EventP_ID_18 0x40000U |
| Event ID 18. More... | |
| #define | EventP_ID_19 0x80000U |
| Event ID 19. More... | |
| #define | EventP_ID_20 0x100000U |
| Event ID 20. More... | |
| #define | EventP_ID_21 0x200000U |
| Event ID 21. More... | |
| #define | EventP_ID_22 0x400000U |
| Event ID 22. More... | |
| #define | EventP_ID_23 0x800000U |
| Event ID 23. More... | |
Typedefs | |
| typedef void * | EventP_Handle |
| Opaque client reference to an instance of a EventP. More... | |
Functions | |
| EventP_Handle | EventP_create (EventP_Params *params) |
| Function to create an event. More... | |
| EventP_Status | EventP_delete (EventP_Handle *handle) |
| Function to delete an event. More... | |
| void | EventP_Params_init (EventP_Params *params) |
| Initialize params structure to default values. More... | |
| uint32_t | EventP_wait (EventP_Handle handle, uint32_t eventMask, uint8_t waitMode, uint32_t timeout) |
| Function for Event Wait. More... | |
| EventP_Status | EventP_post (EventP_Handle handle, uint32_t eventMask) |
| Function for Event Post. More... | |
| uint32_t | EventP_getPostedEvents (EventP_Handle handle) |
| Function to return Event Posted. More... | |