![]() |
TIOVX User Guide
|
Interface to TI extension APIs. More...
#include <VX/vx.h>#include <VX/vx_khr_pipelining.h>#include <VX/vx_khr_user_data_object.h>#include <VX/vx_khr_bidirectional_parameters.h>#include <TI/tivx_debug.h>#include <TI/tivx_log_rt.h>#include <TI/tivx_kernels.h>#include <TI/tivx_nodes.h>#include <TI/tivx_mem.h>#include <TI/tivx_tensor.h>#include <TI/tivx_ext_raw_image.h>#include <TI/tivx_ext_super_node.h>#include <TI/tivx_soc.h>#include <TI/tivx_log_stats.h>Go to the source code of this file.
Macros | |
| #define | TIVX_TARGET_MAX_NAME (64u) |
| Max possible name of a target. | |
| #define | TIVX_TARGET_HOST "HOST" |
| String to name a OpenVX Host. More... | |
| #define | TIVX_CONFIG_PATH_LENGTH (512u) |
| Max size of config file path. | |
| #define | TIVX_CONTROL_CMD_SEND_TO_ALL_REPLICATED_NODES ((uint32_t)-1) |
| When sending a control command to a replicated node, this can be used to send control command to all replicated node. More... | |
| #define | TIVX_GRAPH_MAX_SUPER_NODES (8u) |
| Max possible super nodes in graph. | |
| #define | TIVX_MAX_DSP_BAM_USER_PLUGINS (8u) |
| Max number of BAM user plugins on DSP (in addition to builtin vxlib plugins) | |
| #define | TIVX_SUPER_NODE_MAX_NODES (16u) |
| Max number of nodes per super node. | |
| #define | TIVX_SUPER_NODE_MAX_EDGES (16u) |
| Max number of edges per super node. | |
| #define | TIVX_SUPER_NODE_MAX_OBJECTS (16u) |
| Max number super node objects supported. | |
| #define | TIVX_PYRAMID_MAX_LEVELS_ORB (17u) |
| Max levels supported for the pyramid. More... | |
| #define | TIVX_MAX_KERNEL_ID (VX_KERNEL_MASK) |
| Max number of kernel ID's. | |
| #define | TIVX_MAX_LIBRARY_ID (VX_LIBRARY(VX_LIBRARY_MASK)) |
| Max number of kernel library ID's. | |
| #define | dimof(x) (sizeof(x)/sizeof(x[0])) |
| Macro to find size of array. | |
Enumerations | |
| enum | tivx_graph_attribute_extensions_e { TIVX_GRAPH_STREAM_EXECUTIONS = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_GRAPH) + 0x0 } |
| TI attribute extensions for the graph object. More... | |
| enum | tivx_node_attribute_extensions_e { TIVX_NODE_TARGET_STRING = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x0, TIVX_NODE_TIMEOUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x1, TIVX_NODE_IS_TIMED_OUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x2 } |
| TI attribute extensions for the node object. More... | |
| enum | tivx_reference_attribute_extensions_e { TIVX_REFERENCE_TIMESTAMP = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x0, TIVX_REFERENCE_INVALID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x1, TIVX_REFERENCE_BUFFER_IS_ALLOCATED = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x2 } |
| TI attribute extensions for the reference object. More... | |
| enum | tivx_kernel_attribute_extensions_e { TIVX_KERNEL_TIMEOUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_KERNEL) + 0x0 } |
| TI attribute extensions for the kernel object. More... | |
| enum | tivx_context_attribute_extensions_e { TIVX_CONTEXT_NUM_USER_KERNEL_ID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_CONTEXT) + 0x0, TIVX_CONTEXT_NUM_USER_LIBRARY_ID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_CONTEXT) + 0x1 } |
| TI attribute extensions for the context object. More... | |
| enum | tivx_image_attribute_extensions_e { TIVX_IMAGE_IMAGEPATCH_ADDRESSING = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_IMAGE) + 0x0, TIVX_IMAGE_STRIDE_Y_ALIGNMENT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_IMAGE) + 0x1 } |
| TI attribute extensions for the image object. More... | |
| enum | tivx_tensor_attribute_extensions_e { TIVX_TENSOR_STRIDES = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_TENSOR) + 0x0 } |
| TI attribute extensions for the tensor object. More... | |
| enum | tivx_df_image_e { TIVX_DF_IMAGE_P12 = VX_DF_IMAGE('P','0','1','2'), TIVX_DF_IMAGE_NV12_P12 = VX_DF_IMAGE('N','1','2','P'), TIVX_DF_IMAGE_RGB565 = VX_DF_IMAGE('R','5','6','5'), TIVX_DF_IMAGE_BGRX = VX_DF_IMAGE('B','G','R','A') } |
| Based on the VX_DF_IMAGE definition. More... | |
| enum | tivx_status_e { TIVX_STATUS_BASE = -(vx_int32)100 } |
| The enumeration of all TIVX operational error codes. More... | |
Functions | |
| void | tivxInit (void) |
| Function to initialize OpenVX framework. More... | |
| void | tivxDeInit (void) |
| Function to de-initialize OpenVX framework. More... | |
| void | tivxHostInit (void) |
| Function to initialize OpenVX HOST side functionality. More... | |
| void | tivxHostDeInit (void) |
| Function to de-initialize OpenVX HOST side functionality. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxAddKernelTarget (vx_kernel kernel, const char *target_name) |
| Associate a target with a kernel. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetKernelSinkDepth (vx_kernel kernel, uint32_t num_sink_bufs) |
| Set the number of sink buffers. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxRegisterModule (const char *name, vx_publish_kernels_f publish, vx_unpublish_kernels_f unpublish) |
| Register publish and unpublish functions against a module name. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxUnRegisterModule (const char *name) |
| UnRegister publish and unpublish functions if previously registered. More... | |
| vx_enum | tivxGetSelfCpuId (void) |
| Return CPU ID of the CPU on which this API is called. More... | |
| vx_node | tivxCreateNodeByKernelEnum (vx_graph graph, vx_enum kernelenum, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel enum. More... | |
| vx_node | tivxCreateNodeByKernelRef (vx_graph graph, vx_kernel kernel, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel reference. More... | |
| vx_node | tivxCreateNodeByKernelName (vx_graph graph, const char *kernel_name, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel name. More... | |
| vx_bool | tivxIsReferenceVirtual (vx_reference ref) |
| Utility function to check if the given reference is virtual or not. More... | |
| vx_reference | tivxGetReferenceParent (vx_reference child_ref) |
| Utility function to extract the parent reference from an element. More... | |
| vx_bool | tivxIsTargetEnabled (const char target_name[]) |
| Utility function to know if target is enabled or not. More... | |
| uint64_t | tivxPlatformGetTimeInUsecs (void) |
| Get the time in micro seconds. More... | |
| vx_status VX_API_CALL | tivxSetNodeParameterNumBufByIndex (vx_node node, vx_uint32 idx, vx_uint32 num_buf) |
| Set number of buffers to allocate at output of a node parameter. More... | |
| vx_status VX_API_CALL | tivxGetNodeParameterNumBufByIndex (vx_node node, vx_uint32 idx, vx_uint32 *num_buf) |
| Get number of buffers to allocate at output of a node parameter. More... | |
| vx_status VX_API_CALL | tivxSetGraphPipelineDepth (vx_graph graph, vx_uint32 pipeline_depth) |
| Indicates to the implementation the depth of the graph pipeline. More... | |
| vx_status VX_API_CALL | tivxNodeSendCommand (vx_node node, uint32_t replicate_nodex_idx, uint32_t node_cmd_id, vx_reference ref[], uint32_t num_refs) |
| Send node specific Control command. More... | |
| vx_status VX_API_CALL | tivxNodeSendCommandTimed (vx_node node, uint32_t replicate_nodex_idx, uint32_t node_cmd_id, vx_reference ref[], uint32_t num_refs, uint32_t timeout) |
| Send node specific Control command. More... | |
| vx_node | tivxGraphGetNode (vx_graph graph, uint32_t idx) |
| This API is used to get a reference to a node within a graph at a given index within the graph. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetNodeTileSize (vx_node node, vx_uint32 block_width, vx_uint32 block_height) |
| Sets the tile size for a given node in a graph. This is only valid for BAM-enabled kernels on C66 DSP. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetReferenceAttribute (vx_reference ref, vx_enum attribute, const void *ptr, vx_size size) |
| Sets reference attributes for the below enums: TIVX_REFERENCE_TIMESTAMP. More... | |
| VX_API_ENTRY vx_bool VX_API_CALL | tivxIsReferenceMetaFormatEqual (vx_reference ref1, vx_reference ref2) |
| Check for equivalence between the meta formats of two reference objects. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxReferenceImportHandle (vx_reference ref, const void *addr[], const uint32_t size[], uint32_t num_entries) |
| Updates a reference object with the supplied handles (pointers to memory). More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxReferenceExportHandle (const vx_reference ref, void *addr[], uint32_t size[], uint32_t max_num_entries, uint32_t *num_entries) |
| Exports the handles from a reference object. More... | |
| VX_API_ENTRY vx_reference VX_API_CALL | tivxCreateReferenceFromExemplar (vx_context context, vx_reference exemplar) |
| Create reference from a exemplar object. More... | |
Interface to TI extension APIs.
Definition in file tivx.h.