TIOVX User Guide

Detailed Description

Internal APIs for graph operations.

Data Structures

struct  tivx_graph_t
 The top level data for graph object. More...
 

Functions

int32_t ownGraphGetFreeNodeIndex (vx_graph graph)
 Get next free node entry in graph. More...
 
vx_status ownGraphAddNode (vx_graph graph, vx_node node, int32_t idx)
 Add's a node to a graph. More...
 
vx_status ownGraphRemoveNode (vx_graph graph, vx_node node)
 Remove a node from a graph. More...
 
void ownGraphTopologicalSort (tivx_graph_sort_context *context, vx_node *nodes, uint32_t num_nodes, vx_bool *has_cycle)
 Perform topological sort of graph nodes. More...
 
vx_uint32 ownGraphGetPipeDepth (vx_graph graph)
 Query the leaf nodes of the graph for their depth to find the total depth of the graph. More...
 
vx_bool ownGraphCheckIsRefMatch (vx_graph graph, vx_reference ref1, vx_reference ref2)
 Abstracted check for checking if references match "vx_true_e" will be returned if references match or if references parent object matches. More...
 
void ownGraphSetReverify (vx_graph graph)
 Mark graph to be reverified.
 
tivx_data_ref_queue ownGraphGetParameterDataRefQueue (vx_graph graph, vx_uint32 graph_parameter_index)
 If a data ref queue is associated with 'graph_parameter_index' return it. More...
 
vx_status ownGraphAllocAndEnqueueObjDescForPipeline (vx_graph graph)
 Alloc and enqueue graph obj desc based on graph pipeline depth.
 
vx_status ownGraphAllocForStreaming (vx_graph graph)
 Alloc objects for graph streaming.
 
vx_status ownGraphVerifyStreamingMode (vx_graph graph)
 verify graph schedule mode with streaming
 
vx_status ownGraphFreeObjDesc (vx_graph graph)
 Free graph obj desc based allocated during ownGraphAllocAndEnqueueObjDescForPipeline()
 
vx_status ownGraphFreeStreaming (vx_graph graph)
 Free graph streaming objects.
 
vx_status ownGraphCreateQueues (vx_graph graph)
 Create queues to maintain submitted graph desc and free graph desc.
 
vx_status ownGraphDeleteQueues (vx_graph graph)
 Delete queues created during ownGraphCreateQueues.
 
vx_status ownGraphScheduleGraph (vx_graph graph, uint32_t num_schedule)
 Schedule a graph for execution 'num_schedule' times.
 
vx_status ownGraphScheduleGraphWrapper (vx_graph graph)
 Wrapper for ownGraphScheduleGraph.
 
vx_bool ownCheckGraphCompleted (vx_graph graph, uint32_t pipeline_id)
 Check if a previously scheduled graph execution is complete. More...
 
vx_bool ownGraphDoScheduleGraphAfterEnqueue (vx_graph graph, uint32_t graph_parameter_index)
 Check if a graph should be scheduled after a graph parameter has been enqueued. More...
 
vx_status ownUpdateGraphPerf (vx_graph graph, uint32_t pipeline_id)
 Update graph performance.
 
void ownGraphClearState (vx_graph graph, uint32_t pipeline_id)
 Graph execution state for given pipeline ID.
 
void ownSetGraphState (vx_graph graph, uint32_t pipeline_id, vx_enum state)
 Set graph state for a given pipeline ID.
 
vx_status ownGraphRegisterCompletionEvent (vx_graph graph, vx_uint32 app_value, vx_bool is_context_event)
 Register event on graph completion.
 
vx_status ownGraphRegisterParameterConsumedEvent (vx_graph graph, uint32_t graph_parameter_index, vx_uint32 app_value, vx_bool is_context_event)
 Register event on graph parameter consumed.
 
void ownSendGraphCompletedEvent (vx_graph graph)
 Send graph completion event if enabled.
 
uint32_t ownGraphGetNumSchedule (vx_graph graph)
 Counts number of enqueued 'refs' and returns number of times graph can be scheduled successfully. More...
 
vx_status ownGraphValidatePipelineParameters (vx_graph graph)
 Checks for invalid pipelining conditions (see: TIOVX-726)
 
void ownGraphDetectAndSetNumBuf (vx_graph graph)
 Sets buffers automatically if not already set (see: TIOVX-903)
 
vx_status ownSendUserGraphEvent (vx_graph graph, vx_uint32 app_value, const void *parameter)
 Sends user event to graph event queue.
 
vx_status ownWaitGraphEvent (vx_graph graph, vx_event_t *event, vx_bool do_not_block)
 Waits for user event from graph event queue.
 
vx_status ownGraphAllocateDataObject (vx_node node_cur, uint32_t prm_cur_idx, vx_reference ref)
 Allocates data for an object during verification or graph parameter substitution.
 

Function Documentation

◆ ownGraphGetFreeNodeIndex()

int32_t ownGraphGetFreeNodeIndex ( vx_graph  graph)

Get next free node entry in graph.

Parameters
graph[in] graph object
Returns
0 or more value, index of node in graph
-1, all nodes in graph are used and free node not found

◆ ownGraphAddNode()

vx_status ownGraphAddNode ( vx_graph  graph,
vx_node  node,
int32_t  idx 
)

Add's a node to a graph.

'index' should be the one that is returned via ownGraphGetFreeNodeIndex()

Parameters
graph[in] graph object
node[in] the node to add
idx[in] the index in graph at which to add the node
Returns
VX_SUCCESS, on success

◆ ownGraphRemoveNode()

vx_status ownGraphRemoveNode ( vx_graph  graph,
vx_node  node 
)

Remove a node from a graph.

Parameters
graph[in] graph object
node[in] the node to remove
Returns
VX_SUCCESS, on success

◆ ownGraphTopologicalSort()

void ownGraphTopologicalSort ( tivx_graph_sort_context context,
vx_node nodes,
uint32_t  num_nodes,
vx_bool has_cycle 
)

Perform topological sort of graph nodes.

Parameters
context[in] context to use while sorting
nodes[in,out] IN: Unsorted node, OUT: Sorted nodes
num_nodes[in] Number of nodes
has_cycle[out] vx_true_e: Graph has cycles and cannot be sorted vx_false_e: Graph is acyclic and nodes[] contains the sorted nodes

◆ ownGraphGetPipeDepth()

vx_uint32 ownGraphGetPipeDepth ( vx_graph  graph)

Query the leaf nodes of the graph for their depth to find the total depth of the graph.

Parameters
graph[in] graph object
Returns
Calculated pipe depth

◆ ownGraphCheckIsRefMatch()

vx_bool ownGraphCheckIsRefMatch ( vx_graph  graph,
vx_reference  ref1,
vx_reference  ref2 
)

Abstracted check for checking if references match "vx_true_e" will be returned if references match or if references parent object matches.

Parameters
graph[in] graph in which to check if refs match
ref1[in] first reference
ref2[in] second reference

◆ ownGraphGetParameterDataRefQueue()

tivx_data_ref_queue ownGraphGetParameterDataRefQueue ( vx_graph  graph,
vx_uint32  graph_parameter_index 
)

If a data ref queue is associated with 'graph_parameter_index' return it.

If a data ref queue is NOT associated with 'graph_parameter_index' NULL is returned

◆ ownCheckGraphCompleted()

vx_bool ownCheckGraphCompleted ( vx_graph  graph,
uint32_t  pipeline_id 
)

Check if a previously scheduled graph execution is complete.

Called every time a leaf node completes execution. When all leaf nodes complete execution a graph is said to be completed

◆ ownGraphDoScheduleGraphAfterEnqueue()

vx_bool ownGraphDoScheduleGraphAfterEnqueue ( vx_graph  graph,
uint32_t  graph_parameter_index 
)

Check if a graph should be scheduled after a graph parameter has been enqueued.

This returns true only when graph execution mode is VX_GRAPH_SCHEDULE_MODE_QUEUE_AUTO and graph_parameter_index is the graph parameter which acts as a trigger for auto scheduling.

◆ ownGraphGetNumSchedule()

uint32_t ownGraphGetNumSchedule ( vx_graph  graph)

Counts number of enqueued 'refs' and returns number of times graph can be scheduled successfully.

Value returned is minimum of number of refs enqueued at each graph parameter Valid only in VX_GRAPH_SCHEDULE_MODE_QUEUE_MANUAL mode