TIOVX User Guide

Detailed Description

Context static configuration values.

Defines

#define TIVX_CONTEXT_MAX_CONVOLUTION_DIM   (9)
 The largest convolution matrix the specification requires support for is 9x9.
 
#define TIVX_CONTEXT_MAX_OPTICALFLOWPYRLK_DIM   (9)
 The largest optical flow pyr LK window.
 
#define TIVX_CONTEXT_MAX_NONLINEAR_DIM   (9)
 The largest nonlinear filter matrix the specification requires support for is 9x9.
 
#define TIVX_CONTEXT_MAX_OBJECTS   (1u)
 Max number context objects supported.
 
#define TIVX_CONTEXT_MAX_KERNELS   (128u)
 Max possible unique kernels in a context.
 
#define TIVX_CONTEXT_MAX_USER_STRUCTS   (128u)
 Max possible user structs in a context.
 
#define TIVX_CONTEXT_MAX_REFERENCES
 Max possible references in a context.