![]() |
TIOVX User Guide
|
Helper APIs used used for host side kernel validation.
Defines | |
| #define | TIVX_KERNEL_COMMON_VALID_RECT_MAX_IMAGE (5u) |
| Maximum number of images (input/output) supported in calculating valid rectangles. More... | |
| #define | TIVX_KERNEL_OBJ_ARRAY_SPLIT_NAME "com.ti.ext.obj_array_split" |
| Object Array Split Kernel Name. | |
Functions | |
| vx_status | tivxPublishKernels (vx_context context, const Tivx_Host_Kernel_List *kernel_list, uint32_t num_kernels) |
| Publishes the kernels list on the host side. | |
| vx_status | tivxUnPublishKernels (vx_context context, const Tivx_Host_Kernel_List *kernel_list, uint32_t num_kernels) |
| Unpublishes the kernels list on the host side. | |
| static void | tivxKernelValidRectParams_init (tivxKernelValidRectParams *prms) |
| Function to initialize Valid Rect Parameter structure Currently the entire structure is memset to 0. More... | |
| vx_status | tivxKernelConfigValidRect (tivxKernelValidRectParams *prms) |
| Function to calculate and configure valid region This API loops over all the input and output image's valid rectangles and figures out overlapping rectangle and sets it as valid rectangle in the output image. More... | |
| vx_status | tivxKernelsHostUtilsAddKernelTargetDsp (vx_kernel kernel) |
| Function to add platform-specific DSP kernel target. More... | |
| vx_status | tivxKernelsHostUtilsAddKernelTargetMcu (vx_kernel kernel) |
| Function to add platform-specific R5F kernel target. More... | |
| void | tivxExtLoadKernels (vx_context context) |
| Used for the Application to load the OpenVX Extension kernels into the context. More... | |
| void | tivxExtUnLoadKernels (vx_context context) |
| Used for the Application to unload the OpenVX Extension kernels from the context. More... | |
| #define TIVX_KERNEL_COMMON_VALID_RECT_MAX_IMAGE (5u) |
Maximum number of images (input/output) supported in calculating valid rectangles.
Definition at line 107 of file tivx_kernels_host_utils.h.
|
inlinestatic |
Function to initialize Valid Rect Parameter structure Currently the entire structure is memset to 0.
| prms | [in] Valid Rectange Parameters |
STATIC INLINE FUNCTION DEFINITIONS
Definition at line 196 of file tivx_kernels_host_utils.h.
| vx_status tivxKernelConfigValidRect | ( | tivxKernelValidRectParams * | prms | ) |
Function to calculate and configure valid region This API loops over all the input and output image's valid rectangles and figures out overlapping rectangle and sets it as valid rectangle in the output image.
Each kernel may also require few lines/pixels of padding on each side of the image. Host side kernel can provide this information to this API and it will adjust valid rectangle considering padding requirement also.
This is utility API.
| prms | [in] Valid Rectange Parameters |
Function to add platform-specific DSP kernel target.
Cores which are assigned per SoC are below: J721E: TIVX_TARGET_DSP1 and TIVX_TARGET_DSP2 J721S2: TIVX_TARGET_DSP1 J784S4: TIVX_TARGET_DSP1 J722S: TIVX_TARGET_DSP1 and TIVX_TARGET_DSP2 AM62A: TIVX_TARGET_DSP1
Function to add platform-specific R5F kernel target.
Cores which are assigned per SoC are below: J721E: TIVX_TARGET_MCU2_0 and TIVX_TARGET_MCU2_1 J721S2: TIVX_TARGET_MCU2_0 and TIVX_TARGET_MCU2_1 J784S4: TIVX_TARGET_MCU2_0 and TIVX_TARGET_MCU2_1 J722S: TIVX_TARGET_MCU2_0 and TIVX_TARGET_MCU1_0 AM62A: TIVX_TARGET_MCU1_0
| void tivxExtLoadKernels | ( | vx_context | context | ) |
Used for the Application to load the OpenVX Extension kernels into the context.
This includes object array split kernel
| void tivxExtUnLoadKernels | ( | vx_context | context | ) |
Used for the Application to unload the OpenVX Extension kernels from the context.
This includes object array split kernel