Declarations for PTK_Point and PTK_Vector struct+functions.
|
| void | PTK_Point_set (PTK_Point *dst, float x, float y, float z) |
| | Updates all three components stored within the given PTK_Point to match those given as arguments, to be used primarily for convenience when initializing a point. More...
|
| |
| void | PTK_Vector_add (PTK_Vector *dst, const PTK_Vector *src1, const PTK_Vector *src2) |
| | Perform component-wise addition of the vectors stored in src1 and src2, writing the result to dst. More...
|
| |
| void | PTK_Vector_subtract (PTK_Vector *dst, const PTK_Vector *src1, const PTK_Vector *src2) |
| | Perform component-wise subtraction, subtracting src2 from src1 and writing the result to dst. More...
|
| |
| void | PTK_Vector_scale (PTK_Vector *dst, const PTK_Vector *src, float scale) |
| | Perform component-wise scaling of the given PTK Vector and store the result at dst. More...
|
| |
| void | PTK_Point_transform (PTK_Point *dst, const PTK_Point *src, const PTK_RigidTransform *M) |
| | Perform a rigid transformation on the given point, d = (Mr*s) + Mt. More...
|
| |
| float | PTK_Vector_dot2 (const PTK_Vector *p1, const PTK_Vector *p2) |
| | Compute the dot product of the two given vectors in 2D, given by r = ax*bx + ay*by. More...
|
| |
| float | PTK_Vector_dot3 (const PTK_Vector *p1, const PTK_Vector *p2) |
| | Compute the dot product of the two given vectors in 3D, given by r = ax*bx + ay*by + az*bz. More...
|
| |
| float | PTK_Vector_dot4 (const PTK_Vector *p1, const PTK_Vector *p2) |
| | Compute the dot product of the two given vectors in 3D, given by r = ax*bx + ay*by + az*bz + aw*bw. More...
|
| |
| void | PTK_Vector_computeCrossProduct (PTK_Vector *__restrict dst, const PTK_Vector *__restrict a, const PTK_Vector *__restrict b) |
| | Computes the cross product of the two given vectors in 3D, given by rx = ay*bz - az*by ry = az*bx - ax*bz rz = ax*by - ay*bx. More...
|
| |
| float | PTK_Vector_computeNorm (const PTK_Vector *v) |
| | Computes the L2 norm of the given vector, given by v = sqrt(vx*vx + vy*vy + vz*vz). More...
|
| |
| float | PTK_Vector_normalize (PTK_Vector *__restrict dst, const PTK_Vector *__restrict in) |
| | Normalizes the given input vector and writes to an output vector. More...
|
| |
| void | PTK_Point_tag (PTK_Point *pt, uint32_t tag) |
| | This sets tag bits for the given point. More...
|
| |
| void | PTK_Point_untag (PTK_Point *pt, uint32_t tag) |
| | This removes tag bits for the given point. More...
|
| |
| uint32_t | PTK_Point_isTagged (PTK_Point *pt, uint32_t tag) |
| | This checks if all of the bits set in tag are also set in the tag for the given PTK_Point. Additional bits may be set, but none may be missing from the given mask. More...
|
| |
| void | PTK_Point_d_set (PTK_Point_d *dst, double x, double y, double z) |
| | Updates all three components stored within the given PTK_Point to match those given as arguments, to be used primarily for convenience when initializing a point. More...
|
| |
| void | PTK_Vector_d_add (PTK_Vector_d *dst, PTK_Vector_d *src1, PTK_Vector_d *src2) |
| | Perform component-wise addition of the vectors stored in src1 and src2, writing the result to dst. More...
|
| |
| void | PTK_Vector_d_subtract (PTK_Vector_d *dst, PTK_Vector_d *src1, PTK_Vector_d *src2) |
| | Perform component-wise subtraction, subtracting src2 from src1 and writing the result to dst. More...
|
| |
| void | PTK_Vector_d_scale (PTK_Vector_d *dst, PTK_Vector_d *src, double scale) |
| | Perform component-wise scaling of the given PTK Vector and store the result at dst. More...
|
| |
| void | PTK_Point_d_transform (PTK_Point_d *dst, PTK_Point_d *src, const PTK_RigidTransform_d *M) |
| | Perform a rigid transformation on the given point, d = (Mr*s) + Mt. More...
|
| |
| double | PTK_Vector_d_dot2 (const PTK_Vector_d *p1, const PTK_Vector_d *p2) |
| | Compute the dot product of the two given vectors in 2D, given by r = ax*bx + ay*by. More...
|
| |
| double | PTK_Vector_d_dot3 (const PTK_Vector_d *p1, const PTK_Vector_d *p2) |
| | Compute the dot product of the two given vectors in 3D, given by r = ax*bx + ay*by + az*bz. More...
|
| |
| double | PTK_Vector_d_dot4 (const PTK_Vector_d *p1, const PTK_Vector_d *p2) |
| | Compute the dot product of the two given vectors in 3D, given by r = ax*bx + ay*by + az*bz + aw*bw. More...
|
| |
| void | PTK_Point_d_tag (PTK_Point_d *pt, uint32_t tag) |
| | This sets tag bits for the given point. More...
|
| |
| void | PTK_Point_d_untag (PTK_Point_d *pt, uint32_t tag) |
| | This removes tag bits for the given point. More...
|
| |
| uint32_t | PTK_Point_d_isTagged (PTK_Point_d *pt, uint32_t tag) |
| | This checks if all of the bits set in tag are also set in the tag for the given PTK_Point. Additional bits may be set, but none may be missing from the given mask. More...
|
| |