![]() |
TI J721E Imaging User Guide
|
Data Fields | |
| uint32_t | aeMode |
| uint32_t | digitalGain |
| uint32_t | analogGain |
| uint32_t | expTime |
| uint32_t | awbMode |
| uint32_t | rGain |
| uint32_t | gGain |
| uint32_t | bGain |
| uint32_t | colorTemp |
| uint32_t | awb_valid |
| uint32_t | awb_converged |
| uint32_t AlgItt_IssAewb2AParams::aeMode |
AE Mode, used to enable/disable AE. It could be either AUTO (0) or manual (1), Auto mode is default and runs the AE algorithms Manual mode uses below AE parameters value as AE output
| uint32_t AlgItt_IssAewb2AParams::digitalGain |
Digital Gain for manual AE mode
| uint32_t AlgItt_IssAewb2AParams::analogGain |
Analog Gain for manual AE mode
| uint32_t AlgItt_IssAewb2AParams::expTime |
Exposure time for manual AE mode
| uint32_t AlgItt_IssAewb2AParams::awbMode |
AWB Mode, used to enable/disable AWB. It could be either AUTO (0) or manual (1), Auto mode is default and runs the AWB algorithms Manual mode uses below AWB parameters value as AE output
| uint32_t AlgItt_IssAewb2AParams::rGain |
Red color gain for manual AWB mode
| uint32_t AlgItt_IssAewb2AParams::gGain |
Green color gain for manual AWB mode
| uint32_t AlgItt_IssAewb2AParams::bGain |
Blue color gain for manual AWB mode
| uint32_t AlgItt_IssAewb2AParams::colorTemp |
Color Temperature for manual AWB mode
| uint32_t AlgItt_IssAewb2AParams::awb_valid |
AWB valid
| uint32_t AlgItt_IssAewb2AParams::awb_converged |
AWB converged