![]() |
VXLIB User Guide
|
Structure containing the parameters to initialize the kernel.
Definition at line 82 of file VXLIB_accumulateImage.h.
Data Fields | |
| int8_t | funcStyle |
| Variant of the function, refer to VXLIB_FUNCTION_STYLE More... | |
| VXLIB_OVERFLOW_POLICY | overFlowPolicy |
| Overflow policy, refer to VXLIB_OVERFLOW_POLICY More... | |
| int8_t VXLIB_accumulateImage_InitArgs::funcStyle |
Variant of the function, refer to VXLIB_FUNCTION_STYLE
Definition at line 84 of file VXLIB_accumulateImage.h.
| VXLIB_OVERFLOW_POLICY VXLIB_accumulateImage_InitArgs::overFlowPolicy |
Overflow policy, refer to VXLIB_OVERFLOW_POLICY
Definition at line 86 of file VXLIB_accumulateImage.h.