This section documents the kernels defined for Image Pre/Post Processing.
Data Structures | |
| struct | tivxImgPreProcParams |
| struct | tivxOCPreProcParams |
| struct | tivxOCPostProcParams |
| struct | tivxOCPostProcOutput |
| struct | tivxODPostProcParams |
| struct | tivxDofPlaneSepParams |
| struct | tivxVisualLocalizationParams |
| struct | tivxPixelVizParams |
| struct | tivxImgMosaicParams |
| struct | tivxDrawKeypointDetectionsParams |
| struct | tivxDrawBoxDetectionsParams |
| struct | tivxSFMParams |
| SFM frame level control parameter. More... | |
| struct | tivxDLPreProcParams |
| DL Pre processing to be used with DL-RT. More... | |
| struct | tivxDLColorBlendParams |
| DL color blend to be used with DL-RT. More... | |
| struct | tivxDLRectangle |
| DL rectangles to be used with DL Draw Box. More... | |
| struct | tivxDLDrawBoxParams |
| DL draw box to be used with DL-RT. More... | |
Functions | |
| void | tivxImgProcLoadKernels (vx_context context) |
| Used for the Application to load the img_proc kernels into the context. More... | |
| void | tivxImgProcUnLoadKernels (vx_context context) |
| Used for the Application to unload the img_proc kernels from the context. More... | |
| vx_kernel | tivxAddKernelPixelViz (vx_context context, vx_int32 num_output_tensors) |
| Used for the Application to create the pix viz kernel from the context. More... | |
| vx_kernel | tivxAddKernelImgMosaic (vx_context context, vx_int32 num_inputs) |
| Used by the application to create the mosaic kernel from the context. More... | |
| void | tivxImgMosaicParamsSetDefaults (tivxImgMosaicParams *prms) |
| Set default parameters for tivxImgMosaicParams. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxImgPreProcNode (vx_graph graph, vx_array config, vx_image in_img, vx_tensor out_tensor) |
| Creates a Image Pre Processing Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxOCPreProcNode (vx_graph graph, vx_user_data_object config, vx_image in_img, vx_tensor out_tensor) |
| Creates a OC Pre Processing Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxOCPostProcNode (vx_graph graph, vx_user_data_object config, vx_user_data_object in_args, vx_tensor in_tensor, vx_user_data_object results) |
| Creates a OC Post Processing Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxODPostProcNode (vx_graph graph, vx_array configuration, vx_tensor input_key_points, vx_tensor fwd_table_tensor, vx_tensor rev_table_tensor, vx_tensor kp_tensor, vx_tensor kp_valid) |
| Creates a Post processing Node for Parking Spot Detection Algorithm. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDofPlaneSepNode (vx_graph graph, vx_user_data_object config, vx_image dof_flow, vx_tensor out_planes) |
| Creates a Dense Optical Flow (Dof) 3 plane creation Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxPixelVizNode (vx_graph graph, vx_kernel kernel, vx_user_data_object configuration, vx_user_data_object tidl_out_args, vx_image in_img, vx_int32 num_output_tensors, vx_tensor detection[], vx_image out_img[]) |
| Creates an image with pixel level detection/label overlayed. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxVisualLocalizationNode (vx_graph graph, vx_array configuration, vx_tensor voxel_info, vx_tensor map_3d_points, vx_tensor map_desc, vx_tensor ext_feat_pt, vx_tensor ext_feat_desc, vx_tensor up_samp_wt, vx_tensor lens_dist_table, vx_user_data_object tidl_out_args, vx_matrix pose_tensor) |
| Estimating the camera location from captured image and map information. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxPoseVizNode (vx_graph graph, vx_array configuration, vx_image background_image, vx_matrix pose_tensor, vx_image output_image) |
| Visualization of the estimated location. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxImgMosaicNode (vx_graph graph, vx_kernel kernel, vx_user_data_object config, vx_image output_image, vx_image background_image, vx_object_array input_arr[], vx_uint32 num_inputs) |
| Image Mosiac Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDrawKeypointDetectionsNode (vx_graph graph, vx_user_data_object configuration, vx_tensor kp_tensor, vx_tensor kp_valid, vx_tensor input_tensor, vx_image input_image, vx_image output_image) |
| Draw Keypoint Detections Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDrawBoxDetectionsNode (vx_graph graph, vx_user_data_object configuration, vx_tensor input_tensor, vx_image input_image, vx_image output_image) |
| Draw Box Detections Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxImgHistNode (vx_graph graph, vx_image input_image, vx_distribution output_histogram) |
| Image Histogram Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxSFMNode (vx_graph graph, vx_user_data_object config, vx_user_data_object create_params, vx_user_data_object in_args, vx_user_data_object out_args, vx_image input_image, vx_image flow_vectors, vx_image output_ptcld_image, vx_image output_og_image, vx_user_data_object output_feat) |
| Structure From Motion Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDLPreProcNode (vx_graph graph, vx_user_data_object config, vx_image input_image, vx_tensor output_tensor) |
| DL Pre-processing Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDLColorBlendNode (vx_graph graph, vx_user_data_object config, vx_image input_image, vx_tensor input_tensor, vx_image output_image) |
| DL Color Blend Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDLDrawBoxNode (vx_graph graph, vx_user_data_object config, vx_image input_image, vx_tensor input_tensor, vx_image output_image) |
| DL Draw Box Node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxDLColorConvertNode (vx_graph graph, vx_image input_image, vx_image output_image) |
| DL Color Convert Node. More... | |
Macros | |
| #define | TIVX_MODULE_NAME_IMG_PROC "img_proc" |
| OpenVX module name. More... | |
| #define | TIVX_PIXEL_VIZ_MAX_TENSOR (3U) |
| #define TIVX_MODULE_NAME_IMG_PROC "img_proc" |
OpenVX module name.
| #define TIVX_PIXEL_VIZ_MAX_TENSOR (3U) |
| void tivxImgProcLoadKernels | ( | vx_context | context | ) |
Used for the Application to load the img_proc kernels into the context.
| void tivxImgProcUnLoadKernels | ( | vx_context | context | ) |
Used for the Application to unload the img_proc kernels from the context.
| vx_kernel tivxAddKernelPixelViz | ( | vx_context | context, |
| vx_int32 | num_output_tensors | ||
| ) |
Used for the Application to create the pix viz kernel from the context.
| vx_kernel tivxAddKernelImgMosaic | ( | vx_context | context, |
| vx_int32 | num_inputs | ||
| ) |
Used by the application to create the mosaic kernel from the context.
| void tivxImgMosaicParamsSetDefaults | ( | tivxImgMosaicParams * | prms | ) |
Set default parameters for tivxImgMosaicParams.
| VX_API_ENTRY vx_node VX_API_CALL tivxImgPreProcNode | ( | vx_graph | graph, |
| vx_array | config, | ||
| vx_image | in_img, | ||
| vx_tensor | out_tensor | ||
| ) |
Creates a Image Pre Processing Node.
Node does pre processing needed for conventional deep learning algorithm. Preprocessing steps such as mean subtraction, scaling and plane deinterleaving is supported by this Node.
| [in] | graph | The reference to the graph. |
| [in] | config | Array element type tivxImgPreProcParams, max number of elements = 1 |
| [in] | in_img | input image |
| [in] | out_tensor | output tensor |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxOCPreProcNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_image | in_img, | ||
| vx_tensor | out_tensor | ||
| ) |
Creates a OC Pre Processing Node.
Node does pre processing needed for image classification operation Performs only NV12 to BGR conversion
| [in] | graph | The reference to the graph. |
| [in] | config | User data object element type tivxOCPreProcParams |
| [in] | in_img | input image |
| [out] | out_tensor | output tensor |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxOCPostProcNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_user_data_object | in_args, | ||
| vx_tensor | in_tensor, | ||
| vx_user_data_object | results | ||
| ) |
Creates a OC Post Processing Node.
Node does post processing needed for conventional image classification algorithm. Returns top N classes from a list of probabilities
| [in] | graph | The reference to the graph. |
| [in] | config | User data object element type tivxOCPostProcParams |
| [in] | in_args | input user data object |
| [in] | in_tensor | input tensor |
| [out] | results | output user data object |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxODPostProcNode | ( | vx_graph | graph, |
| vx_array | configuration, | ||
| vx_tensor | input_key_points, | ||
| vx_tensor | fwd_table_tensor, | ||
| vx_tensor | rev_table_tensor, | ||
| vx_tensor | kp_tensor, | ||
| vx_tensor | kp_valid | ||
| ) |
Creates a Post processing Node for Parking Spot Detection Algorithm.
Node does generates interpolated points on parking spot periphery from four corners points detected from deep learning based algorithm
| [in] | graph | The reference to the graph. |
| [in] | configuration | Array element type tivxODPostProcParams, max number of elements = 1 |
| [in] | input_key_points | Interleaved 4 corner points of multiple parking spots. |
| [in] | fwd_table_tensor | Angular map table for rectilinear angle to fish eye angle |
| [in] | rev_table_tensor | Angular map table for fish eye angle to rectilinear angle |
| [in] | kp_tensor | output interpolated points on periphery of parking spot |
| [in] | kp_valid | output flag of validity for each parking spot |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDofPlaneSepNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_image | dof_flow, | ||
| vx_tensor | out_planes | ||
| ) |
Creates a Dense Optical Flow (Dof) 3 plane creation Node.
Node does creation of three planes (each of 8 bit) from the raw 32 bit output from Dof hardware accelerator 3 planes corresponds to horizontal, vertical flow vectors and confidence
| [in] | graph | The reference to the graph. |
| [in] | config | Array element type tivxDofPlaneSepParams, max number of elements = 1 |
| [in] | dof_flow | input dof flow vectors |
| [out] | out_planes | output planes. |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxPixelVizNode | ( | vx_graph | graph, |
| vx_kernel | kernel, | ||
| vx_user_data_object | configuration, | ||
| vx_user_data_object | tidl_out_args, | ||
| vx_image | in_img, | ||
| vx_int32 | num_output_tensors, | ||
| vx_tensor | detection[], | ||
| vx_image | out_img[] | ||
| ) |
Creates an image with pixel level detection/label overlayed.
Node does blending of input image with pixel level detection/classification data for visualization purpose.
| [in] | graph | The reference to the graph. |
| [in] | kernel | The reference to openvx kernel |
| [in] | configuration | Array element type tivxODPostProcParams, max number of elements = 1 |
| [in] | tidl_out_args | out args of tidl to receive the scale values of each output tensor |
| [in] | in_img | Input image. |
| [in] | num_output_tensors | Number of output tensors/images. |
| [in] | detection | Detection planes |
| [out] | out_img | ovelayed output image |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxVisualLocalizationNode | ( | vx_graph | graph, |
| vx_array | configuration, | ||
| vx_tensor | voxel_info, | ||
| vx_tensor | map_3d_points, | ||
| vx_tensor | map_desc, | ||
| vx_tensor | ext_feat_pt, | ||
| vx_tensor | ext_feat_desc, | ||
| vx_tensor | up_samp_wt, | ||
| vx_tensor | lens_dist_table, | ||
| vx_user_data_object | tidl_out_args, | ||
| vx_matrix | pose_tensor | ||
| ) |
Estimating the camera location from captured image and map information.
Node estimates the location in 3d world co-ordinate
| [in] | graph | The reference to the graph. |
| [in] | configuration | Array element type tivxODPostProcParams, max number of elements = 1 |
| [in] | voxel_info | Voxel info. voxels are cuboid in real world |
| [in] | map_3d_points | Map 3D points |
| [in] | map_desc | Map descriptors |
| [in] | ext_feat_pt | Externally computed feature points(x,y) |
| [in] | ext_feat_desc | Feature descriptor for each feature point |
| [in] | up_samp_wt | Filter weights for upsampling |
| [in] | lens_dist_table | Fish eye lens distortion table |
| [in] | tidl_out_args | TIDL outatgs needed for scale |
| [out] | pose_tensor | Output pose matrix of size 3x4 |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxPoseVizNode | ( | vx_graph | graph, |
| vx_array | configuration, | ||
| vx_image | background_image, | ||
| vx_matrix | pose_tensor, | ||
| vx_image | output_image | ||
| ) |
Visualization of the estimated location.
Node generated an image with visualization of X, Y location of 3D world on image plane
| [in] | graph | The reference to the graph. |
| [in] | configuration | Array element type tivxODPostProcParams, max number of elements = 1 |
| [in] | background_image | Background image on which pose information will be visualized |
| [in] | pose_tensor | Input pose matrix created by tivxVisualLocalizationNode Node |
| [out] | output_image | Output image |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxImgMosaicNode | ( | vx_graph | graph, |
| vx_kernel | kernel, | ||
| vx_user_data_object | config, | ||
| vx_image | output_image, | ||
| vx_image | background_image, | ||
| vx_object_array | input_arr[], | ||
| vx_uint32 | num_inputs | ||
| ) |
Image Mosiac Node.
Used to mosiac a list of images onto to a sigle image
| [in] | graph | The reference to the graph. |
| [in] | kernel | The reference to the openvx kernel |
| [in] | config | Mosaic configuration of type tivxImgMosaicParams |
| [out] | output_image | Output image of type vx_image, only VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8, VX_DF_IMAGE_U16 supported |
| [in] | background_image | Optional background image of type vx_image, only VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8, VX_DF_IMAGE_U16 supported |
| [in] | input_arr | Array of inputs of type vx_image, only VX_DF_IMAGE_NV12, VX_DF_IMAGE_U8, VX_DF_IMAGE_U16 supported |
| [in] | num_inputs | Number of inputs, i.e number of elements in input_arr[] |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDrawKeypointDetectionsNode | ( | vx_graph | graph, |
| vx_user_data_object | configuration, | ||
| vx_tensor | kp_tensor, | ||
| vx_tensor | kp_valid, | ||
| vx_tensor | input_tensor, | ||
| vx_image | input_image, | ||
| vx_image | output_image | ||
| ) |
Draw Keypoint Detections Node.
Used to draw keypoint detections on an image
| [in] | graph | reference to the graph. |
| [in] | configuration | configuration of type tivxDrawKeyPointDetectionParams |
| [in] | kp_tensor | keypoint tensor from OD postprocessing node |
| [in] | kp_valid | valid keypoints tensor from OD postprocessing node |
| [in] | input_tensor | TIDL output tensor of detected key points |
| [in] | input_image | Input image to draw detections |
| [out] | output_image | Output image with detections drawn |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDrawBoxDetectionsNode | ( | vx_graph | graph, |
| vx_user_data_object | configuration, | ||
| vx_tensor | input_tensor, | ||
| vx_image | input_image, | ||
| vx_image | output_image | ||
| ) |
Draw Box Detections Node.
Used to draw box detections on an image
| [in] | graph | reference to the graph. |
| [in] | configuration | configuration of type tivxDrawBoxDetectionParams |
| [in] | input_tensor | TIDL output tensor of detected key points |
| [in] | input_image | Input image to draw detections |
| [out] | output_image | Output image with detections drawn |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxImgHistNode | ( | vx_graph | graph, |
| vx_image | input_image, | ||
| vx_distribution | output_histogram | ||
| ) |
Image Histogram Node.
Used to get histogram of image intensity, done on A72
| [in] | graph | reference to the graph. |
| [in] | input_image | Input image to draw detections |
| [out] | output_histogram | Output histogram of image intensities (luma only) |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxSFMNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_user_data_object | create_params, | ||
| vx_user_data_object | in_args, | ||
| vx_user_data_object | out_args, | ||
| vx_image | input_image, | ||
| vx_image | flow_vectors, | ||
| vx_image | output_ptcld_image, | ||
| vx_image | output_og_image, | ||
| vx_user_data_object | output_feat | ||
| ) |
Structure From Motion Node.
Structure From Motion (SFM), done on C71
| [in] | graph | reference to the graph. |
| [in] | config | SFM parameters defined in tivxSFMParams |
| [in] | create_params | SFM parameters defined in tivxSFMParams |
| [in] | in_args | SFM parameters defined in tivxSFMParams |
| [in] | out_args | SFM parameters defined in tivxSFMParams |
| [in] | input_image | Input image in NV12 format to overlay depth estimations |
| [in] | flow_vectors | Flow vectors in VX_DF_IMAGE_U32 format |
| [out] | output_ptcld_image | Output point cloud image |
| [out] | output_og_image | Output occupancy grid map |
| [out] | output_feat | Output features |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDLPreProcNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_image | input_image, | ||
| vx_tensor | output_tensor | ||
| ) |
DL Pre-processing Node.
Transforms input image to a format as required for DL processing
| [in] | graph | reference to the graph |
| [in] | config | reference to tivxDLPreProcPrams |
| [in] | input_image | Input image |
| [out] | output_tensor | Output tensor |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDLColorBlendNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_image | input_image, | ||
| vx_tensor | input_tensor, | ||
| vx_image | output_image | ||
| ) |
DL Color Blend Node.
Takes the DL output and blends the provided color-map to the input image
| [in] | graph | reference to the graph |
| [in] | config | reference to tivxDLPreProcPrams |
| [in] | input_image | Input image |
| [in] | input_tensor | Input tensor |
| [out] | output_image | Output image |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDLDrawBoxNode | ( | vx_graph | graph, |
| vx_user_data_object | config, | ||
| vx_image | input_image, | ||
| vx_tensor | input_tensor, | ||
| vx_image | output_image | ||
| ) |
DL Draw Box Node.
Takes the DL output and draws boxes around an object on input image
| [in] | graph | reference to the graph |
| [in] | config | reference to tivxDLPreProcPrams |
| [in] | input_image | Input image |
| [in] | input_tensor | Input tensor |
| [out] | output_image | Output image |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| VX_API_ENTRY vx_node VX_API_CALL tivxDLColorConvertNode | ( | vx_graph | graph, |
| vx_image | input_image, | ||
| vx_image | output_image | ||
| ) |
DL Color Convert Node.
Performs limited color conversions required for DL pipeline which is DMA optimized
| [in] | graph | reference to the graph |
| [in] | input_image | Input image |
| [out] | output_image | Output image |
| vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |