35 #define TIVX_DEFAULT_TILE_HEIGHT (48u) 40 #define TIVX_DEFAULT_TILE_WIDTH (64u) 45 typedef struct _vx_node {
vx_bool local_data_set_allow
Flag to indicate if local data size and ptr set is allowed.
vx_bool is_kernel_created
to check if kernel is created
vx_bool local_data_ptr_is_alloc
flag to indicate if local_data_ptr is allocated by system TRUE: allocated by system (TIOVX implementa...
vx_status ownNodeKernelInitKernelName(vx_node node)
Init user kernel or target kernel name associated with this node.
vx_bool is_graph_streaming_node_completion_event
flag to indicate whether event is using streaming event queue for graph streaming ...
vx_bool is_enable_send_complete_event
when true a event is sent when a node execution is completed
vx_action(* vx_nodecomplete_f)(vx_node node)
vx_status ownNodeAddInNode(vx_node node, vx_node out_node)
Associate a input node with a given node.
vx_status ownSetNodeImmTarget(vx_node node)
Set the target for node based on immediate mode target set in context.
void ownNodeLinkArrayElement(vx_node node, uint32_t prm_id)
Link array element to node at parameter index 'prm_id'.
The most basic type in the OpenVX system. Any type that inherits from tivx_reference_t must have a vx...
uint32_t node_error_graph_app_value
Value returned with node error event for graph events.
vx_status ownNodeKernelDeinitKernelName(vx_node node)
Deinit user kernel or target kernel name associated with this node.
vx_status ownNodeSetParameter(vx_node node, vx_uint32 idx, vx_reference value)
Set parameter at node.
vx_status ownNodeAllocObjDescForPipeline(vx_node node, uint32_t pipeline_depth)
Alloc additional node obj desc's for pipelining.
vx_bool is_initialized
flag to indicate if node has been initialized
tivx_reference_t base
The internal reference object.
struct _vx_meta_format * vx_meta_format
vx_bool is_context_error_event
flag to indicate whether error event is using context event queue
uint32_t node_completed_context_app_value
Value returned with node completion event for context events.
struct _vx_reference * vx_reference
vx_status ownNodeRegisterEvent(vx_node node, vx_enum event_type, vx_uint32 app_value, enum tivx_queue_type_e queue_type)
Register node completion event.
vx_status ownNodeKernelDeinit(vx_node node)
DeInit user kernel or target kernel associated with this node.
vx_status ownUpdateNodePerf(vx_node node, uint32_t pipeline_id)
Called by graph each time after node execution.
vx_bool is_graph_node_completion_event
flag to indicate whether event is using graph event queue for node completion events ...
vx_status ownNodeKernelSchedule(vx_node node, uint32_t pipeline_id)
Schedule user kernel or target kernel associated with this node for execution.
vx_perf_t perf
Node performance.
vx_action ownNodeExecuteUserCallback(vx_node node)
Call user specified callback.
uint32_t pipeline_depth
pipeline depth of graph this node belongs to
void * local_data_ptr
local data pointer
vx_status ownNodeKernelInit(vx_node node)
Init user kernel or target kernel associated with this node.
uint32_t ownNodeGetParameterNumBuf(vx_node node, vx_uint32 idx)
Return number of buffers to allocate at a node,index.
vx_bool is_timed_out
flag to indicate whether node has timed out
vx_graph graph
The pointer to parent graph.
vx_uint32 node_depth
Depth of a given node.
vx_reference ownNodeGetParameterRef(vx_node node, uint32_t prm_index)
Get reference associated with a parameters of a parameter.
vx_bool is_enable_send_error_event
when true a event is sent when a node execution is completed and is an error
void ownNodeSetObjDescParamDirection(vx_node node)
Set param direction for 0th node obj desc.
Command object descriptor.
void ownNodeCheckAndSendCompletionEvent(const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp)
Send node completion event if enabled.
struct _tivx_super_node * tivx_super_node
The Super Node Framework Object. Super Node is a strongly-typed container for connected nodes...
struct _vx_kernel * vx_kernel
struct _tivx_data_ref_queue * tivx_data_ref_queue
Data Ref Queue Object.
uint32_t ownNodeGetNumParameters(vx_node node)
Return number of node parameters.
vx_status ownNodeCreateUserCallbackCommand(vx_node node, uint32_t pipeline_id)
Create resources required to call a user callback If user callback is assigned then nothing is done...
vx_status ownNodeReplaceOutNode(vx_node node, vx_node old_out_node, vx_node new_out_node)
Replace an output node for a given node with a new output node.
uint32_t ownNodeGetNumInNodes(vx_node node)
Get number of input nodes associated with this node.
vx_status ownNodeUserKernelExecute(vx_node node, vx_reference prm_ref[])
Execute user kernel.
vx_bool valid_rect_reset
reset valid rectangle
void ownNodeClearExecuteState(vx_node node, uint32_t pipeline_id)
clears execute status of the node
vx_status ownNodeAddOutNode(vx_node node, vx_node out_node)
Associate a output node with a given node.
uint32_t node_completed_graph_streaming_app_value
Value returned with node completion event for graph streaming events.
vx_status ownResetNodePerf(vx_node node)
Reset node performance statistics.
tivx_queue_type_e
Type of event that can be generated during system execution.
uint32_t ownNodeGetNumOutNodes(vx_node node)
Get number of output nodes associated with this node.
The internal representation of a node.
vx_node ownNodeGetNextNode(vx_node node, vx_uint32 idx)
Get next node at given output index.
void ownNodeLinkObjDescForPipeline(vx_node node)
Update in node id and out node id for node pipeline obj desc's.
uint16_t incounter
used by graph topological sort for internal state keeping
#define TIVX_GRAPH_MAX_PIPELINE_DEPTH
Max possible pipeline depth of a graph.
tivx_super_node super_node
The pointer to the super node that this node references.
uint32_t node_completed_graph_app_value
Value returned with node completion event for graph events.
vx_bool is_context_completion_event
flag to indicate whether completion event is using context event queue
vx_uint32 timeout_val
Control API processing Timeout value in milli-sec.
#define TIVX_KERNEL_MAX_PARAMS
Max parameters in a kernel This is required to be <= 32 per framework requirements.
struct _vx_graph * vx_graph
vx_status ownNodeReplaceInNode(vx_node node, vx_node old_in_node, vx_node new_in_node)
Replace an input node for a given node with a new input node.
vx_bool is_super_node
flag to indicate whether node is a placeholder for a super node
uint32_t node_error_context_app_value
Value returned with node error event for context events.
struct _vx_node * vx_node
vx_bool ownNodeIsPrmReplicated(vx_node node, uint32_t prm_idx)
Is prm_idx of node replicated.
vx_kernel kernel
The pointer to the kernel structure.
vx_nodecomplete_f user_callback
Node completion callback.
void ownNodeLinkDataRefQueue(vx_node node, uint32_t prm_id, tivx_data_ref_queue data_ref_q)
Link data ref q to node at parameter index 'prm_id'.
vx_status ownSetNodeAttributeValidRectReset(vx_node node, vx_bool is_reset)
Set the attribute VX_NODE_VALID_RECT_RESET in node.
uint32_t node_error_graph_streaming_app_value
Value returned with node error event for graph streaming events.
vx_enum ownNodeGetParameterDir(vx_node node, uint32_t prm_index)
Get direction of a parameter.
vx_status ownNodeKernelValidate(vx_node node, vx_meta_format meta[])
Validate user kernel or target kernel associated with this node.
void ownNodeCheckAndSendErrorEvent(const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp, vx_status status)
Send node error event if node failed.
vx_size local_data_size
local data size
vx_node ownNodeGetNextInNode(vx_node node, vx_uint32 idx)
Get next node at given input index.
vx_bool is_graph_error_event
flag to indicate whether event is using graph event queue for node error events