19 #ifndef VX_META_FORMAT_H_ 20 #define VX_META_FORMAT_H_ 37 typedef struct _vx_meta_format
#define VX_MAX_REFERENCE_NAME
vx_status(* vx_kernel_image_valid_rectangle_f)(vx_node node, vx_uint32 index, const vx_rectangle_t *const input_valid[], vx_rectangle_t *const output_valid[])
The most basic type in the OpenVX system. Any type that inherits from tivx_reference_t must have a vx...
struct _vx_context * vx_context
struct _vx_meta_format * vx_meta_format
#define TIVX_CONTEXT_MAX_TENSOR_DIMS
Max possible dimensions of data in a tensor.
The raw image create params structure that is given to the tivxCreateRawImage function.