![]() |
TIOVX User Guide
|
Enumerations for configuration output routing in VPAC VISS structures.
Defines | |
| #define | TIVX_VPAC_VISS_FCP1_DISABLED (0U) |
| #define | TIVX_VPAC_VISS_FCP1_INPUT_RFE (1U) |
| #define | TIVX_VPAC_VISS_FCP1_INPUT_CAC (2U) |
| #define | TIVX_VPAC_VISS_FCP1_INPUT_NSF4 (3U) |
| #define | TIVX_VPAC_VISS_FCP1_INPUT_GLBCE (4U) |
| #define | TIVX_VPAC_VISS_FCP0 (0U) |
| #define | TIVX_VPAC_VISS_FCP1 (1U) |
| #define | TIVX_VPAC_VISS_FCP_OUT0 (0U) |
| #define | TIVX_VPAC_VISS_FCP_OUT1 (0U) |
| #define | TIVX_VPAC_VISS_FCP_OUT2 (1U) |
| #define | TIVX_VPAC_VISS_FCP_OUT3 (1U) |
| #define | TIVX_VPAC_VISS_FCP_OUT4 (0U) |
| #define | TIVX_VPAC_VISS_MAP_FCP_OUTPUT(fcp, output) (output<<1 | fcp) |
| #define TIVX_VPAC_VISS_FCP1_DISABLED (0U) |
Definition at line 92 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP1_INPUT_RFE (1U) |
Definition at line 94 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP1_INPUT_CAC (2U) |
Definition at line 96 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP1_INPUT_NSF4 (3U) |
Definition at line 98 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP1_INPUT_GLBCE (4U) |
Definition at line 100 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP0 (0U) |
Definition at line 103 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP1 (1U) |
Definition at line 105 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP_OUT0 (0U) |
Definition at line 108 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP_OUT1 (0U) |
Definition at line 110 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP_OUT2 (1U) |
Definition at line 112 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP_OUT3 (1U) |
Definition at line 114 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_FCP_OUT4 (0U) |
Definition at line 116 of file hwa_vpac_viss3.h.
| #define TIVX_VPAC_VISS_MAP_FCP_OUTPUT | ( | fcp, | |
| output | |||
| ) | (output<<1 | fcp) |
Macro to set the output_fcp_mapping
Definition at line 120 of file hwa_vpac_viss3.h.