![]() |
TIOVX User Guide
|
APIs creating and using tensor data type (note: this is not included in OpenVX 1.1 and thus added to TI extensions)
Typedefs | |
| typedef struct _vx_tensor * | vx_tensor |
| The multidimensional data object (Tensor). More... | |
Enumerations | |
| enum | vx_tensor_attribute_e { VX_TENSOR_NUMBER_OF_DIMS = VX_ATTRIBUTE_BASE( VX_ID_KHRONOS, VX_TYPE_TENSOR ) + 0x0, VX_TENSOR_DIMS = VX_ATTRIBUTE_BASE( VX_ID_KHRONOS, VX_TYPE_TENSOR ) + 0x1, VX_TENSOR_DATA_TYPE = VX_ATTRIBUTE_BASE( VX_ID_KHRONOS, VX_TYPE_TENSOR ) + 0x2, VX_TENSOR_FIXED_POINT_POSITION = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_TENSOR) + 0x3, TIVX_TENSOR_SCALING_DIVISOR = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_TENSOR) + 0x4, TIVX_TENSOR_SCALING_DIVISOR_FIXED_POINT_POSITION = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_TENSOR) + 0x5 } |
| tensor Data attributes. More... | |
Functions | |
| VX_API_ENTRY vx_tensor VX_API_CALL | vxCreateTensor (vx_context context, vx_size number_of_dims, const vx_size *dims, vx_enum data_type, vx_int8 fixed_point_position) |
| Creates an opaque reference to a tensor data buffer. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxCopyTensorPatch (vx_tensor tensor, vx_size number_of_dims, const vx_size *view_start, const vx_size *view_end, const vx_size *user_stride, void *user_ptr, vx_enum usage, vx_enum user_memory_type) |
| Allows the application to copy a view patch from/into an tensor object . More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxQueryTensor (vx_tensor tensor, vx_enum attribute, void *ptr, vx_size size) |
| Retrieves various attributes of a tensor data. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxSetTensorAttribute (vx_tensor tensor, vx_enum attribute, const void *ptr, vx_size size) |
| Sets attributes of a tensor object. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxReleaseTensor (vx_tensor *tensor) |
| Releases a reference to a tensor data object. The object may not be garbage collected until its total reference count is zero. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxUnmapTensorPatch (vx_tensor tensor, vx_map_id map_id) |
| Unmap and commit potential changes to a tensor object patch that were previously mapped. Unmapping a tensor patch invalidates the memory location from which the patch could be accessed by the application. Accessing this memory location after the unmap function completes has an undefined behavior. More... | |
| typedef struct _vx_tensor* vx_tensor |
The multidimensional data object (Tensor).
Definition at line 89 of file tivx_tensor.h.
tensor Data attributes.
Definition at line 109 of file tivx_tensor.h.
| VX_API_ENTRY vx_tensor VX_API_CALL vxCreateTensor | ( | vx_context | context, |
| vx_size | number_of_dims, | ||
| const vx_size * | dims, | ||
| vx_enum | data_type, | ||
| vx_int8 | fixed_point_position | ||
| ) |
Creates an opaque reference to a tensor data buffer.
Not guaranteed to exist until the vx_graph containing it has been verified. Since functions using tensors, need to understand the context of each dimension. We describe a layout of the dimensions in each function using tensors. That layout is not mandatory. It is done specifically to explain the functions and not to mandate layout. Different implementation may have different layout. Therefore the layout description is logical and not physical. It refers to the order of dimensions given in this function.
| [in] | context | The reference to the implementation context. |
| [in] | number_of_dims | The number of dimensions. |
| [in] | dims | Dimensions sizes in elements. |
| [in] | data_type | The vx_type_e that represents the data type of the tensor data elements. |
| [in] | fixed_point_position | Specifies the fixed point position when the input element type is integer. if 0, calculations are performed in integer math. |
vxGetStatus. | VX_API_ENTRY vx_status VX_API_CALL vxCopyTensorPatch | ( | vx_tensor | tensor, |
| vx_size | number_of_dims, | ||
| const vx_size * | view_start, | ||
| const vx_size * | view_end, | ||
| const vx_size * | user_stride, | ||
| void * | user_ptr, | ||
| vx_enum | usage, | ||
| vx_enum | user_memory_type | ||
| ) |
Allows the application to copy a view patch from/into an tensor object .
| [in] | tensor | The reference to the tensor object that is the source or the destination of the copy. |
| [in] | number_of_dims | Number of patch dimension. Error return if 0 or greater than number of tensor dimensions. If smaller than number of tensor dimensions, the lower dimensions are assumed. |
| [in] | view_start | Array of patch start points in each dimension |
| [in] | view_end | Array of patch end points in each dimension |
| [in] | user_stride | Array of user memory strides in each dimension |
| [in] | user_ptr | The address of the memory location where to store the requested data if the copy was requested in read mode, or from where to get the data to store into the tensor object if the copy was requested in write mode. The accessible memory must be large enough to contain the specified patch with the specified layout: accessible memory in bytes >= (end[last_dimension] - start[last_dimension]) * stride[last_dimension]. The layout of the user memory must follow a row major order. |
| [in] | usage | This declares the effect of the copy with regard to the tensor object using the vx_accessor_e enumeration. Only VX_READ_ONLY and VX_WRITE_ONLY are supported:
|
| [in] | user_memory_type | A vx_memory_type_e enumeration that specifies the memory type of the memory referenced by the user_addr. |
vx_status_e enumeration. | VX_ERROR_OPTIMIZED_AWAY | This is a reference to a virtual tensor that cannot be accessed by the application. |
| VX_ERROR_INVALID_REFERENCE | The tensor reference is not actually an tensor reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxQueryTensor | ( | vx_tensor | tensor, |
| vx_enum | attribute, | ||
| void * | ptr, | ||
| vx_size | size | ||
| ) |
Retrieves various attributes of a tensor data.
| [in] | tensor | The reference to the tensor data to query. |
| [in] | attribute | The attribute to query. Use a vx_tensor_attribute_e. |
| [out] | ptr | The location at which to store the resulting value. |
| [in] | size | The size of the container to which ptr points. |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | If data is not a vx_tensor. |
| VX_ERROR_INVALID_PARAMETERS | If any of the other parameters are incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxSetTensorAttribute | ( | vx_tensor | tensor, |
| vx_enum | attribute, | ||
| const void * | ptr, | ||
| vx_size | size | ||
| ) |
Sets attributes of a tensor object.
| [in] | tensor | The tensor object to set. |
| [in] | attribute | The attribute to modify. Use a vx_tensor_attribute_e enumeration. |
| [in] | ptr | The pointer to the value to which to set the attribute. |
| [in] | size | The size of the data pointed to by ptr. |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | If data is not a vx_tensor. |
| VX_ERROR_INVALID_PARAMETERS | If any of the other parameters are incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxReleaseTensor | ( | vx_tensor * | tensor | ) |
Releases a reference to a tensor data object. The object may not be garbage collected until its total reference count is zero.
| [in] | tensor | The pointer to the tensor data to release. |
vx_status_e enumeration. | VX_SUCCESS | No errors; all other values indicate failure |
| * | An error occurred. See vx_status_e. |
| VX_API_ENTRY vx_status VX_API_CALL tivxUnmapTensorPatch | ( | vx_tensor | tensor, |
| vx_map_id | map_id | ||
| ) |
Unmap and commit potential changes to a tensor object patch that were previously mapped. Unmapping a tensor patch invalidates the memory location from which the patch could be accessed by the application. Accessing this memory location after the unmap function completes has an undefined behavior.
| [in] | tensor | The reference to the tensor object to unmap. |
| [out] | map_id | The unique map identifier that was returned by tivxMapTensorPatch . |
vx_status_e enumeration. | VX_ERROR_INVALID_REFERENCE | The tensor reference is not actually a tensor reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
tivxMapTensorPatch with same map_id value