TIOVX User Guide
tiovx.kernel_code.KernelExportCode Class Reference

Code object used to generate custom kernel. More...

Public Member Functions

def __init__ (self, module="ext1", core="c66", env_var='VISION_APPS_PATH', include_subpath="TI", include_filename="")
 Constructor used to create this object. More...
 
def exportDiagram (self, kernel)
 Export object as C source code.
 
def export (self, kernel)
 Method for generating files from kernel. More...
 

Detailed Description

Code object used to generate custom kernel.

Example Usage: Setting up file paths for custom kernel
Note: if leaving the optional field for env_var blank, you must set CUSTOM_KERNEL_PATH
from tiovx import *
code = KernelExportCode(Module.IMAGING, Core.C66, "CUSTOM_KERNEL_PATH")
<set up kernel parameters>
code.export(kernel)

Output files from the above parameters:

<CUSTOM_KERNEL_PATH>/DEVELOPER_TODO.txt (generated first time only for given parameters)
<CUSTOM_KERNEL_PATH>/include/TI/tivx_imaging.h (generated first time only for given parameters)
<CUSTOM_KERNEL_PATH>/include/TI/tivx_imaging_kernels.h (generated first time only for given parameters)
<CUSTOM_KERNEL_PATH>/include/TI/tivx_imaging_nodes.h (generated first time only for given parameters)

Output folder from the above parameters:

<CUSTOM_KERNEL_PATH>/imaging/

This folder contains the following:

c66/concerto.mak (generated first time only for given parameters)
c66/vx_<kernel_name>_target.c
c66/vx_kernels_imaging_target.c (generated first time only for given parameters)
c66/bam/vx_bam_<kernel_name>_target.c (if using the C66 DSP)
c66/bam/concerto.mak (generated first time only for given parameters, if using the C66 DSP)
host/concerto.mak (generated first time only for given parameters)
tivx_imaging_node_api.c (generated first time only for given parameters)
host/vx_<kernel_name>_host.c
host/vx_kernels_imaging_host.c (generated first time only for given parameters)
include/tivx_imaging_kernels.h (generated first time only for given parameters)
include/tivx_kernel_<kernel_name>.h
test/concerto.mak (generated first time only for given parameters)
test/test_main.h (generated first time only for given parameters)
Below is an example using the CUSTOM_APPLICATION_PATH
from tiovx import *
code = KernelExportCode(Module.IMAGING, Core.C66, "CUSTOM_APPLICATION_PATH")
<set up kernel parameters>
code.export(kernel)

Output files from the above parameters:

<CUSTOM_APPLICATION_PATH>/DEVELOPER_TODO.txt
<CUSTOM_APPLICATION_PATH>/concerto_inc.mak
<CUSTOM_APPLICATION_PATH>/custom_tools_path.mak
<CUSTOM_APPLICATION_PATH>/kernels/imaging/include/TI/tivx_imaging.h
<CUSTOM_APPLICATION_PATH>/kernels/imaging/include/TI/tivx_imaging_kernels.h
<CUSTOM_APPLICATION_PATH>/kernels/imaging/include/TI/tivx_imaging_nodes.h

Output folder from the above parameters:

<CUSTOM_APPLICATION_PATH>/kernels/imaging/

This folder contains the following:

c66/concerto.mak (generated first time only for given parameters)
c66/vx_<kernel_name>_target.c
c66/vx_kernels_imaging_target.c (generated first time only for given parameters)
c66/bam/vx_bam_<kernel_name>_target.c (if using the C66 DSP)
c66/bam/concerto.mak (generated first time only for given parameters, if using the C66 DSP)
host/concerto.mak (generated first time only for given parameters)
tivx_imaging_node_api.c (generated first time only for given parameters)
host/vx_<kernel_name>_host.c
host/vx_kernels_imaging_host.c (generated first time only for given parameters)
include/tivx_imaging_kernels.h (generated first time only for given parameters)
include/tivx_kernel_<kernel_name>.h
test/concerto.mak (generated first time only for given parameters)
test/test_main.h (generated first time only for given parameters)
Below is an example using the VISION_APPS_PATH
from tiovx import *
code = KernelExportCode(Module.IMAGING, Core.C66, "VISION_APPS_PATH")
<set up kernel parameters>
code.export(kernel)

Output files from the above parameters:

<VISION_APPS_PATH>/kernels/DEVELOPER_TODO.txt
<VISION_APPS_PATH>/kernels/imaging/include/TI/tivx_imaging.h
<VISION_APPS_PATH>/kernels/imaging/include/TI/tivx_imaging_kernels.h
<VISION_APPS_PATH>/kernels/imaging/include/TI/tivx_imaging_nodes.h

Output folder from the above parameters:

<VISION_APPS_PATH>/kernels/imaging/

This folder contains the following:

c66/concerto.mak (generated first time only for given parameters)
c66/vx_<kernel_name>_target.c
c66/vx_kernels_imaging_target.c (generated first time only for given parameters)
c66/bam/vx_bam_<kernel_name>_target.c (if using the C66 DSP)
c66/bam/concerto.mak (generated first time only for given parameters, if using the C66 DSP)
host/concerto.mak (generated first time only for given parameters)
tivx_imaging_node_api.c (generated first time only for given parameters)
host/vx_<kernel_name>_host.c
host/vx_kernels_imaging_host.c (generated first time only for given parameters)
include/tivx_imaging_kernels.h (generated first time only for given parameters)
include/tivx_kernel_<kernel_name>.h
test/concerto.mak (generated first time only for given parameters)
test/test_main.h (generated first time only for given parameters)

Definition at line 194 of file kernel_code.py.

Constructor & Destructor Documentation

◆ __init__()

def tiovx.kernel_code.KernelExportCode.__init__ (   self,
  module = "ext1",
  core = "c66",
  env_var = 'VISION_APPS_PATH',
  include_subpath = "TI",
  include_filename = "" 
)

Constructor used to create this object.

Parameters
module[in] [optional] Module name for the kernel; Default="ext1"
core[in] [optional] Name of the core for the kernel to run on; Default="c66"
env_var[in] [optional] Path to the directory where these should be outputted; Default="VISION_APPS_PATH"
include_subpath[in] [optional] Company name which serves as a subpath for an include directory; Default="TI"
include_filename[in] [optional] Variable to overwrite the include filename, otherwise include filename set to <lowercase(include_subpath)>vx_<module>; Default=""

Definition at line 202 of file kernel_code.py.

Member Function Documentation

◆ export()

def tiovx.kernel_code.KernelExportCode.export (   self,
  kernel 
)

Method for generating files from kernel.

Parameters
kernel[in] Kernel to be exported to a file

Definition at line 3052 of file kernel_code.py.


The documentation for this class was generated from the following file: