Kernel for computing elementwise sine of an input vector. Supports float and double datatype.
◆ MATHLIB_sin()
Performs the elementwise sine of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise sine of the input vector.
- Template Parameters
-
| T | : implementation datatype |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | pSrc | : pointer to buffer holding input vector |
| [out] | pDst | : pointer to buffer holding result vector |
- Returns
- Status of success.
◆ MATHLIB_sin_sp()
| MATHLIB_STATUS MATHLIB_sin_sp |
( |
size_t |
length, |
|
|
float * |
pSrc, |
|
|
float * |
pDst |
|
) |
| |
This function is the C interface for MATHLIB_sin. Function accepts float pointers.
- Template Parameters
-
| T | : implementation datatype |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | pSrc | : pointer to buffer holding input vector |
| [out] | pDst | : pointer to buffer holding result vector |
- Returns
- Status of success.
Definition at line 266 of file MATHLIB_sin.cpp.
◆ MATHLIB_sin_dp()
| MATHLIB_STATUS MATHLIB_sin_dp |
( |
size_t |
length, |
|
|
double * |
pSrc, |
|
|
double * |
pDst |
|
) |
| |
This function is the C interface for MATHLIB_sin. Function accepts double pointers.
- Template Parameters
-
| T | : implementation datatype |
- Parameters
-
| [in] | length | : length of input vector |
| [in] | pSrc | : pointer to buffer holding input vector |
| [out] | pDst | : pointer to buffer holding result vector |
- Returns
- Status of success.
Definition at line 274 of file MATHLIB_sin.cpp.