![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| static void | MATHLIB_SE0SA01DSequentialInit (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, size_t length, T *pSrc, T *pDst) |
| template<typename T > | |
| static void | MATHLIB_SE0SA0Open (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc) |
| This method performs SE0 and SA0 open. More... | |
| template<typename T > | |
| static void | MATHLIB_SE0SE1SA0Open (__SE_TEMPLATE_v1 *se0Params, __SA_TEMPLATE_v1 *sa0Params, T *pSrc0, T *pSrc1) |
| This method performs SE0, SE1, and SA0 open. More... | |
| static void | MATHLIB_SE0SA0Close () |
| This method performs SE0 and SA0 close. More... | |
| static void | MATHLIB_SE0SE1SA0Close () |
| This method performs SE0, SE1, and SA0 close. More... | |
| template<typename T > | |
| static MATHLIB_STATUS | MATHLIB_checkParams (size_t length, T *pSrc, T *pDst) |
| This method performs parameter checks for MATHLIB function. More... | |
| template<typename T > | |
| static MATHLIB_STATUS | MATHLIB_checkParams (size_t length, T *pSrc0, T *pSrc1, T *pDst) |
| static double | cmn_DIVDP (double a, double b) |
| static float | cmn_DIVSP (float a, float b) |