![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_rsqrt (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise reciprocal square root of an input vectors. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise reciprocal square root of an input vector. More... | |
| MATHLIB_STATUS | MATHLIB_rsqrt_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_rsqrt. Function accepts float pointers. More... | |