![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Macros | |
| #define | ELEMENT_COUNT(x) c7x::element_count_of<x>::value |
| #define | ELEMENT_TYPE(x) typename c7x::element_type_of<x>::type |
Functions | |
| template<typename vecType > | |
| static vecType | sqrt_acos_i (vecType a) |
| template<typename vecType > | |
| static vecType | pol_est_acos_i (vecType x) |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_acos (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise arc-cosine of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise arc-cosine of a vector. More... | |
| template MATHLIB_STATUS | MATHLIB_acos< float > (size_t length, float *pSrc, float *pDst) |
| MATHLIB_STATUS | MATHLIB_acos_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_acos. Function accepts float pointers. More... | |
| #define ELEMENT_COUNT | ( | x | ) | c7x::element_count_of<x>::value |
Definition at line 34 of file MATHLIB_acos.cpp.
| #define ELEMENT_TYPE | ( | x | ) | typename c7x::element_type_of<x>::type |
Definition at line 36 of file MATHLIB_acos.cpp.
|
inlinestatic |
Definition at line 59 of file MATHLIB_acos.cpp.
|
inlinestatic |
Definition at line 91 of file MATHLIB_acos.cpp.
| template MATHLIB_STATUS MATHLIB_acos< float > | ( | size_t | length, |
| float * | pSrc, | ||
| float * | pDst | ||
| ) |