![]() |
TI J721E Imaging User Guide
|
Handle to the sensor driver. Includes all the information about the sensor.
Data Fields | |
| uint32_t | isUsed |
| IssSensor_CreateParams * | createPrms |
| IssSensorFxns * | sensorFxns |
| IssSensorIntfParams * | sensorIntfPrms |
| uint32_t IssSensors_Handle::isUsed |
Flag to indicate if given instance is free or not
| IssSensor_CreateParams* IssSensors_Handle::createPrms |
Create Parameters
| IssSensorFxns* IssSensors_Handle::sensorFxns |
Registered Sensor's parameters
| IssSensorIntfParams* IssSensors_Handle::sensorIntfPrms |
Registered Sensor's interface parameters