DSPLIB User Guide
DSPLIB_svd_small_InitArgs Struct Reference

Detailed Description

Structure containing the parameters to initialize the kernel.

Definition at line 137 of file DSPLIB_svd_small.h.

Data Fields

int8_t funcStyle
 Variant of the function refer to DSPLIB_FUNCTION_STYLE
More...
 
uint32_t dimX
 Size of input data dimX => Number of columns ( = 6 or 7) More...
 
uint32_t dimY
 Size of input data dimY => Number of rows ( = 6 only) More...
 
uint32_t enableReducedForm
 Flag to activate reduced form calculation | 1 => REDUCED FORM | 0 => NON-REDUCED FORM. More...
 
uint32_t strideURows
 Stride value for U matrix in the transposed form. More...
 
uint32_t strideVRows
 Stride value for V matrix in the transposed form. More...
 

Field Documentation

◆ funcStyle

int8_t DSPLIB_svd_small_InitArgs::funcStyle

Variant of the function refer to DSPLIB_FUNCTION_STYLE

Definition at line 139 of file DSPLIB_svd_small.h.

◆ dimX

uint32_t DSPLIB_svd_small_InitArgs::dimX

Size of input data dimX => Number of columns ( = 6 or 7)

Definition at line 141 of file DSPLIB_svd_small.h.

◆ dimY

uint32_t DSPLIB_svd_small_InitArgs::dimY

Size of input data dimY => Number of rows ( = 6 only)

Definition at line 143 of file DSPLIB_svd_small.h.

◆ enableReducedForm

uint32_t DSPLIB_svd_small_InitArgs::enableReducedForm

Flag to activate reduced form calculation | 1 => REDUCED FORM | 0 => NON-REDUCED FORM.

Definition at line 145 of file DSPLIB_svd_small.h.

◆ strideURows

uint32_t DSPLIB_svd_small_InitArgs::strideURows

Stride value for U matrix in the transposed form.

Definition at line 147 of file DSPLIB_svd_small.h.

◆ strideVRows

uint32_t DSPLIB_svd_small_InitArgs::strideVRows

Stride value for V matrix in the transposed form.

Definition at line 149 of file DSPLIB_svd_small.h.