![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 169 of file DSPLIB_sqrAdd_priv.h.
Data Fields | |
| pFxnDSPLIB_sqrAdd_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_sqrAdd_exec_cn and DSPLIB_sqrAdd_exec_ci. More... | |
| int32_t | blockSize |
| Size of input buffer for different batches DSPLIB_sqrAdd_init that will be retrieved and used by DSPLIB_sqrAdd_exec More... | |
| uint8_t | bufPblock [DSPLIB_SQRADD_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_sqrAdd_exec DSPLIB_sqrAdd_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_sqrAdd_exec_cn and DSPLIB_sqrAdd_exec_ci.
Definition at line 173 of file DSPLIB_sqrAdd_priv.h.
| int32_t DSPLIB_sqrAdd_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_sqrAdd_init that will be retrieved and used by DSPLIB_sqrAdd_exec
Definition at line 177 of file DSPLIB_sqrAdd_priv.h.
| uint8_t DSPLIB_sqrAdd_PrivArgs::bufPblock[DSPLIB_SQRADD_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 179 of file DSPLIB_sqrAdd_priv.h.