![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 128 of file DSPLIB_recip_priv.h.
Data Fields | |
| pFxnDSPLIB_recip_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_recip_exec_cn and DSPLIB_recip_exec_ci. More... | |
| int32_t | blockSize |
| Size of input buffer for different batches DSPLIB_recip_init that will be retrieved and used by DSPLIB_recip_exec More... | |
| uint8_t | bufPblock [DSPLIB_RECIP_IXX_IXX_OXX_PBLOCK_SIZE] |
| DSPLIB_recip_InitArgs | initArgs |
| pFxnDSPLIB_recip_exec DSPLIB_recip_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_recip_exec_cn and DSPLIB_recip_exec_ci.
Definition at line 132 of file DSPLIB_recip_priv.h.
| int32_t DSPLIB_recip_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_recip_init that will be retrieved and used by DSPLIB_recip_exec
Definition at line 136 of file DSPLIB_recip_priv.h.
| uint8_t DSPLIB_recip_PrivArgs::bufPblock[DSPLIB_RECIP_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 137 of file DSPLIB_recip_priv.h.
| DSPLIB_recip_InitArgs DSPLIB_recip_PrivArgs::initArgs |
Definition at line 140 of file DSPLIB_recip_priv.h.