![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 162 of file DSPLIB_blk_move_priv.h.
Data Fields | |
| pFxnDSPLIB_blk_move_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_blk_move_exec_cn and DSPLIB_blk_move_exec_ci. More... | |
| int32_t | blockSize |
| Size of input buffer for different batches DSPLIB_blk_move_init that will be retrieved and used by DSPLIB_blk_move_exec More... | |
| uint8_t | bufPblock [DSPLIB_BLK_MOVE_IXX_IXX_OXX_PBLOCK_SIZE] |
| Buffer to save SE & SA configuration parameters More... | |
| pFxnDSPLIB_blk_move_exec DSPLIB_blk_move_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_blk_move_exec_cn and DSPLIB_blk_move_exec_ci.
Definition at line 166 of file DSPLIB_blk_move_priv.h.
| int32_t DSPLIB_blk_move_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_blk_move_init that will be retrieved and used by DSPLIB_blk_move_exec
Definition at line 170 of file DSPLIB_blk_move_priv.h.
| uint8_t DSPLIB_blk_move_PrivArgs::bufPblock[DSPLIB_BLK_MOVE_IXX_IXX_OXX_PBLOCK_SIZE] |
Buffer to save SE & SA configuration parameters
Definition at line 172 of file DSPLIB_blk_move_priv.h.