![]() |
DSPLIB User Guide
|
Kernel for multiplying two matrices.
Data Structures | |
| struct | DSPLIB_matMul_fixed_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_matMul_fixed_getHandleSize (DSPLIB_matMul_fixed_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_matMul_fixed_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn0, DSPLIB_bufParams2D_t *bufParamsIn1, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_fixed_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_matMul_fixed_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_matMul_fixed_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn0, const DSPLIB_bufParams2D_t *bufParamsIn1, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_matMul_fixed_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_init function. This function is called with the same parameters as the DSPLIB_matMul_fixed_init, and this function must be called before the DSPLIB_matMul_fixed_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_matMul_fixed_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn0, const void *restrict pIn1, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_exec function. This function is called with the same parameters as the DSPLIB_matMul_fixed_init, and this function must be called before the DSPLIB_matMul_fixed_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_matMul_fixed_exec (DSPLIB_kernelHandle handle, void *restrict pIn0, void *restrict pIn1, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
| int32_t DSPLIB_matMul_fixed_getHandleSize | ( | DSPLIB_matMul_fixed_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 26 of file DSPLIB_matMul_fixed.cpp.
| DSPLIB_STATUS DSPLIB_matMul_fixed_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsIn0, | ||
| DSPLIB_bufParams2D_t * | bufParamsIn1, | ||
| DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_matMul_fixed_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_matMul_fixed_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn0 | : Pointer to the structure containing dimensional information of input matrix A |
| [in] | bufParamsIn1 | : Pointer to the structure containing dimensional information of input matrix B |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output matrix C |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 93 of file DSPLIB_matMul_fixed.cpp.
| DSPLIB_STATUS DSPLIB_matMul_fixed_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn0, | ||
| const DSPLIB_bufParams2D_t * | bufParamsIn1, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_matMul_fixed_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_init function. This function is called with the same parameters as the DSPLIB_matMul_fixed_init, and this function must be called before the DSPLIB_matMul_fixed_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn0 | : Pointer to the structure containing dimensional information of input matrix A |
| [in] | bufParamsIn1 | : Pointer to the structure containing dimensional information of input matrix B |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output matrix C |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 33 of file DSPLIB_matMul_fixed.cpp.
| DSPLIB_STATUS DSPLIB_matMul_fixed_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn0, | ||
| const void *restrict | pIn1, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_matMul_fixed_exec function. This function is called with the same parameters as the DSPLIB_matMul_fixed_init, and this function must be called before the DSPLIB_matMul_fixed_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn0 | : Pointer to the structure input matrix A |
| [in] | pIn1 | : Pointer to the structure input matrix B |
| [out] | pout | : Pointer to the output matrix C |
Definition at line 73 of file DSPLIB_matMul_fixed.cpp.
| DSPLIB_STATUS DSPLIB_matMul_fixed_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn0, | ||
| void *restrict | pIn1, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_matMul_fixed_exec
| [in] | handle | : Active handle to the kernel |
| [in] | pIn0 | : Pointer to buffer holding the input matrix A |
| [in] | pIn1 | : Pointer to buffer holding the input matrix B |
| [out] | pOut | : Pointer to buffer holding the output matrix C |
Definition at line 166 of file DSPLIB_matMul_fixed.cpp.