![]() |
DSPLIB User Guide
|
Kernel for multichannel multistage cascade on input data.
Data Structures | |
| struct | DSPLIB_cascadeBiquad_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_cascadeBiquad_getHandleSize (DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| int32_t | DSPLIB_cascadeBiquad_get_coefficientsBufferSize (uint32_t numStages) |
| This is a query function to calculate the sizes of coefficient buffer needed based on the number of stages. More... | |
| DSPLIB_STATUS | DSPLIB_cascadeBiquad_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsFilterCoeff, DSPLIB_bufParams2D_t *bufParamsFilterVar, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_cascadeBiquad_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_cascadeBiquad_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cascadeBiquad_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_cascadeBiquad_init function. This function is called with the same parameters as the DSPLIB_cascadeBiquad_init, and this function must be called before the DSPLIB_cascadeBiquad_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_cascadeBiquad_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilterCoeff, void *restrict pFilterVar, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
| DSPLIB_STATUS | DSPLIB_cascadeBiquad_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pFilterCoeff, const void *restrict pFilterVar, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_cascadeBiquad_exec function. This function is called with the same parameters as the DSPLIB_cascadeBiquad_exec, and this function must be called before the DSPLIB_cascadeBiquad_exec is called. More... | |
| void | DSPLIB_cascadeBiquad_perfEst (DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsFilterCoeff, const DSPLIB_bufParams2D_t *bufParamsFilterVar, const DSPLIB_bufParams2D_t *bufParamsOut, uint64_t *archCycles, uint64_t *estCycles) |
| This is a utility function that gives an estimate of the cycles consumed for the kernel execution. More... | |
| int32_t DSPLIB_cascadeBiquad_getHandleSize | ( | DSPLIB_cascadeBiquad_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 25 of file DSPLIB_cascadeBiquad.cpp.
| int32_t DSPLIB_cascadeBiquad_get_coefficientsBufferSize | ( | uint32_t | numStages | ) |
This is a query function to calculate the sizes of coefficient buffer needed based on the number of stages.
| [in] | numStages | : number of stages |
Definition at line 102 of file DSPLIB_cascadeBiquad.cpp.
| DSPLIB_STATUS DSPLIB_cascadeBiquad_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsFilterCoeff, | ||
| DSPLIB_bufParams2D_t * | bufParamsFilterVar, | ||
| DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| DSPLIB_cascadeBiquad_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_cascadeBiquad_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 176 of file DSPLIB_cascadeBiquad.cpp.
| DSPLIB_STATUS DSPLIB_cascadeBiquad_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsFilterCoeff, | ||
| const DSPLIB_bufParams2D_t * | bufParamsFilterVar, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| const DSPLIB_cascadeBiquad_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_cascadeBiquad_init function. This function is called with the same parameters as the DSPLIB_cascadeBiquad_init, and this function must be called before the DSPLIB_cascadeBiquad_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of filter buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 31 of file DSPLIB_cascadeBiquad.cpp.
| DSPLIB_STATUS DSPLIB_cascadeBiquad_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pFilterCoeff, | ||
| void *restrict | pFilterVar, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_cascadeBiquad
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the filter data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 243 of file DSPLIB_cascadeBiquad.cpp.
| DSPLIB_STATUS DSPLIB_cascadeBiquad_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn, | ||
| const void *restrict | pFilterCoeff, | ||
| const void *restrict | pFilterVar, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_cascadeBiquad_exec function. This function is called with the same parameters as the DSPLIB_cascadeBiquad_exec, and this function must be called before the DSPLIB_cascadeBiquad_exec is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [in] | pFilter | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output matrix |
Definition at line 68 of file DSPLIB_cascadeBiquad.cpp.
| void DSPLIB_cascadeBiquad_perfEst | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams2D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsFilterCoeff, | ||
| const DSPLIB_bufParams2D_t * | bufParamsFilterVar, | ||
| const DSPLIB_bufParams2D_t * | bufParamsOut, | ||
| uint64_t * | archCycles, | ||
| uint64_t * | estCycles | ||
| ) |
This is a utility function that gives an estimate of the cycles consumed for the kernel execution.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of the input buffer |
| [in] | bufParamsFilter | : Pointer to the structure containing dimensional information of the filter buffer |
| [in] | bufParamsOut | : Pointer to the structure containing dimensional information of the output buffer |
| [out] | archCycles | : Cycles estimated for the compute, startup and teardown |
| [out] | estCycles | : Cycles estimated for the compute, startup, teardown and any associated overhead |