71 if ((pIn == NULL) || (pOut == NULL)) {
139 status = pKerPrivArgs->
execute(handle, pIn, pOut);
template DSPLIB_STATUS DSPLIB_q15tofl_exec_ci< float >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_q15tofl_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_q15tofl_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_q15tofl_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_q15tofl_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_q15tofl_exec_ci< double >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_q15tofl_exec_cn< float >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_q15tofl_exec_cn< double >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_q15tofl_init_cn(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_q15tofl_InitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_q15tofl.
#define DSPLIB_DEBUGPRINTFN(N, fmt,...)
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
@ DSPLIB_ERR_NULL_POINTER
@ DSPLIB_ERR_INVALID_TYPE
DSPLIB_STATUS DSPLIB_q15tofl_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel compute function.
int32_t DSPLIB_q15tofl_getHandleSize(DSPLIB_q15tofl_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_q15tofl_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_q15tofl_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_q15tofl_exec function is called. This function takes...
DSPLIB_STATUS DSPLIB_q15tofl_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_q15tofl_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_q15tofl_init function....
DSPLIB_STATUS DSPLIB_q15tofl_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_q15tofl_exec function....
A structure for a 1 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
uint32_t dataSize
Size of input data
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_q15tofl_exec execute
Function pointer to point to the right execution variant between DSPLIB_q15tofl_exec_cn and DSPLIB_q1...
int32_t blockSize
Size of input buffer for different batches DSPLIB_q15tofl_init that will be retrieved and used by DSP...