21 #ifndef DSPLIB_FIR_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_FIR_IXX_IXX_OXX_PRIV_H_
24 #include "../common/DSPLIB_utility.h"
38 #define DSPLIB_FIR_IXX_IXX_OXX_PBLOCK_SIZE (3 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
47 void *restrict pFilter,
80 template <
typename dataType>
113 template <
typename dataType>
133 template <
typename dataType,
typename accumulateType>
161 template <
typename dataType>
DSPLIB_STATUS DSPLIB_fir_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsFilter, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_fir_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_fir_exec_cn(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_fir_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut, DSPLIB_fir_InitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
DSPLIB_STATUS DSPLIB_fir_exec_ci(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut)
This function is the main execution function for the C7x implementation of the kernel....
#define DSPLIB_FIR_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_fir_PrivArgs structure.
DSPLIB_STATUS(* pFxnDSPLIB_fir_exec)(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pFilter, void *restrict pOut)
This is a function pointer type that conforms to the declaration of DSPLIB_fir_exec_ci and DSPLIB_fir...
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_fir_getSizes(const DSPLIB_fir_InitArgs *pKerInitArgs, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsFilter, DSPLIB_bufParams2D_t *bufParamsOut)
This function is a utility function that the application calls to obtain the sizes of data buffers.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
int32_t remFilterLoopSize
uint32_t flag
Array to store the configuration prepared by DSPLIB_fir_init_ci that will be retrieved and used by DS...
uint32_t dataBufferOutPitch
Pitch of output buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLI...
uint32_t filterPitch
Pitch of filter coefficient buffer for different batches DSPLIB_fir_init that will be retrieved and u...
uint32_t dataBufferInPitch
Pitch of input buffer for different batches DSPLIB_fir_init that will be retrieved and used by DSPLIB...
DSPLIB_fir_InitArgs initArgs
Structure holding initialization parameters
pFxnDSPLIB_fir_exec execute
Function pointer to point to the right execution variant between DSPLIB_fir_exec_cn and DSPLIB_fir_ex...