DSPLIB User Guide
DSPLIB_dotp_sqr_priv.h File Reference

Introduction

Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_dotp_sqr.

Definition in file DSPLIB_dotp_sqr_priv.h.

Go to the source code of this file.

Data Structures

struct  DSPLIB_dotp_sqr_PrivArgs
 Structure that is reserved for internal use by the kernel. More...
 

Macros

#define DSPLIB_DOTP_SQR_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
 Macro to define the size of bufPblock array of DSPLIB_dotp_sqr_PrivArgs structure. More...
 

Typedefs

typedef DSPLIB_STATUS(* pFxnDSPLIB_dotp_sqr_exec) (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
 This is a function pointer type that conforms to the declaration of DSPLIB_dotp_sqr_exec_ci and DSPLIB_dotp_sqr_exec_cn. More...
 

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_dotp_sqr_InitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_exec. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_exec. More...
 
DSPLIB_STATUS DSPLIB_dotp_sqr_init_cn (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut)
 This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_init. More...
 

Macro Definition Documentation

◆ DSPLIB_DOTP_SQR_IXX_IXX_OXX_PBLOCK_SIZE

#define DSPLIB_DOTP_SQR_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))

Macro to define the size of bufPblock array of DSPLIB_dotp_sqr_PrivArgs structure.

Definition at line 39 of file DSPLIB_dotp_sqr_priv.h.

Typedef Documentation

◆ pFxnDSPLIB_dotp_sqr_exec

typedef DSPLIB_STATUS(* pFxnDSPLIB_dotp_sqr_exec) (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pOut)

This is a function pointer type that conforms to the declaration of DSPLIB_dotp_sqr_exec_ci and DSPLIB_dotp_sqr_exec_cn.

Definition at line 45 of file DSPLIB_dotp_sqr_priv.h.

Function Documentation

◆ DSPLIB_dotp_sqr_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_init_ci ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_dotp_sqr_InitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_init.

This function determines the configuration for the streaming engine and MMA hardware resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_dotp_sqr_exec_ci would be called later independently by the application. When DSPLIB_dotp_sqr_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_dotp_sqr_exec_ci does not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 62 of file DSPLIB_dotp_sqr_ci.cpp.

◆ DSPLIB_dotp_sqr_exec_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_exec_ci ( DSPLIB_kernelHandle  handle,
void *restrict  pIn1,
void *restrict  pIn2,
void *restrict  pOut 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_exec.

The function uses MMA hardware accelerator to perform the convolution computation. Filter data is loaded into B panel of the MMA from memory using one streaming engine, while the input data is loaded into A vectors of the MMA using the other streaming engine. Result of the compute from MMA C panel is stored into memory using a stream address generator.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

Definition at line 227 of file DSPLIB_dotp_sqr_ci.cpp.

◆ DSPLIB_dotp_sqr_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_dotp_sqr_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn1,
void *restrict  pIn2,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_exec.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[in]pFilterCoeffPointer to buffer holding the filter coefficient data
[in]pFilterVar: Pointer to buffer holding the filter variable data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 39 of file DSPLIB_dotp_sqr_cn.cpp.

◆ DSPLIB_dotp_sqr_init_cn()

DSPLIB_STATUS DSPLIB_dotp_sqr_init_cn ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams2D_t bufParamsIn,
DSPLIB_bufParams2D_t bufParamsOut 
)

This function is the initialization function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_dotp_sqr_init.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.