DSPLIB User Guide
DSPLIB_cholesky_solver.h File Reference

Go to the source code of this file.

Data Structures

struct  DSPLIB_cholesky_solver_InitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_cholesky_solver_getHandleSize (DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_cholesky_solver_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsU, DSPLIB_bufParams2D_t *bufParamsScratch, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsX, DSPLIB_bufParams1D_t *bufParamsDiv, const DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_cholesky_solver_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_cholesky_solver_init_checkParams (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsU, DSPLIB_bufParams2D_t *bufParamsScratch, DSPLIB_bufParams1D_t *bufParamsY, DSPLIB_bufParams1D_t *bufParamsB, DSPLIB_bufParams1D_t *bufParamsX, DSPLIB_bufParams1D_t *bufParamsDiv, const DSPLIB_cholesky_solver_InitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_cholesky_solver_init function. This function is called with the same parameters as the DSPLIB_cholesky_solver_init, and this function must be called before the DSPLIB_cholesky_solver_init is called. More...
 
DSPLIB_STATUS DSPLIB_cholesky_solver_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pU, const void *restrict pScratch, const void *restrict pY, const void *restrict pB, const void *restrict pX, const void *restrict pDiv)
 This function checks the validity of the parameters passed to DSPLIB_cholesky_solver_exec function. This function is called with the same parameters as the DSPLIB_cholesky_solver_init, and this function must be called before the DSPLIB_cholesky_solver_init is called. More...
 
DSPLIB_STATUS DSPLIB_cholesky_solver_exec (DSPLIB_kernelHandle handle, void *restrict pU, void *restrict pScratch, void *restrict pY, void *restrict pB, void *restrict pX, void *restrict pDiv)
 This function is the main kernel compute function. More...