81 #ifndef DSPLIB_CHOLESKY_IXX_IXX_OXX_H_
82 #define DSPLIB_CHOLESKY_IXX_IXX_OXX_H_
85 #include "../common/DSPLIB_types.h"
201 const void *restrict pInA,
202 const void *restrict pOutU,
203 const void *restrict pMul);
240 void *restrict pOutU,
241 void *restrict pMul);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_cholesky_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pInA, const void *restrict pOutU, const void *restrict pMul)
This function checks the validity of the parameters passed to DSPLIB_cholesky_exec function....
int32_t DSPLIB_cholesky_getHandleSize(DSPLIB_cholesky_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_cholesky_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_cholesky_init function....
DSPLIB_STATUS DSPLIB_cholesky_exec(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict pMul)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_cholesky_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsIn, DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_cholesky_exec function is called....
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
int32_t strideCn
stride of output data in cn
int32_t stride
stride of input/output data in ci
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
int32_t enableTest
Flag to enable Positive definiteness check.
int32_t order
order of input data