DSPLIB User Guide
DSPLIB_blk_eswap.h File Reference

Go to the source code of this file.

Data Structures

struct  DSPLIB_blk_eswap_InitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_blk_eswap_getHandleSize (DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_blk_eswap_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_blk_eswap_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_blk_eswap_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_blk_eswap_init function. This function is called with the same parameters as the DSPLIB_blk_eswap_init, and this function must be called before the DSPLIB_blk_eswap_init is called. More...
 
DSPLIB_STATUS DSPLIB_blk_eswap_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
 This function checks the validity of the parameters passed to DSPLIB_blk_eswap_exec function. This function is called with the same parameters as the DSPLIB_blk_eswap_init, and this function must be called before the DSPLIB_blk_eswap_init is called. More...
 
DSPLIB_STATUS DSPLIB_blk_eswap_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main kernel swapping function. More...