J722S MCU+ SDK  10.01.00
EVM Setup

J722S-EVM

Cable Connections

  • The figure below shows some important cable connections, ports and switches.
    • Take note of the location of the "BOOTMODE" switch, this is used to switch between different boot modes like OSPI, UART, SD, NOBOOT mode

J722S-EVM

Setup UART Terminal

  • Many examples use a standard UART terminal to log the output from the examples. You can use any UART terminal program for the same. Below steps show how to setup the UART terminal from CCS.
  • First identify the UART port as enumerated on the host machine.
  • In CCS, goto "View > Terminal"

UART Terminal Menu
  • Open a new UART terminal

Open New UART Terminal
  • Select the UART port, keep other options to default, i.e 115200 baud rate - 8 data bits - No parity - 1 stop bit,
    • We use the 3rd USB serial port, as seen in the device manager, for below in the SDK
      • Flashing application via UART
      • Booting application via UART
      • Uboot and Linux terminal
    • We use the 3rd USB serial port, as seen in the device manager, as terminal output for examples which run from DM R5F (WKUP R5F)
    • We use the 4th USB serial port, as seen in the device manager, as terminal output for examples which run from MCU R5F

Connect to UART port
  • In this screenshot this happens to be COM27 and COM30. However on your machine this could be different. One tip to make sure there is no mistake in identifying the UART port is to disconnect all other UART to USB devices other than this EVM before checking in device manager.

Flash SOC Initialization Binary

Attention
This is a recommended one time step that needs to be done before you can load and run programs via CCS
If this step fails, maybe due to bad flash in EVM, then try one of the other SOC initialization steps mentioned at SOC Initialization
This step needs to be done once unless the OSPI flash has been erased or some other application has been flashed
These steps are not applicable for HS-SE devices as JTAG can not be connected to HS-SE devices by default. Follow the steps in Flash a Hello World example for flashing the HS-SE device.
  • A quick recap of steps done so far that are needed for the flashing to work
    • Make sure the UART port used for terminal is identified as mentioned in Setup UART Terminal
    • Make sure python3 is installed as mentioned in Python3
    • Make sure you have the EVM power cable and UART cable connected as shown in Cable Connections
  • Build all the binaries from the mcu_plus_sdk installation path.
    • For Linux
        make -sj4 all
      
  • POWER-OFF the EVM
  • Set boot mode to UART BOOTMODE as shown in below image

UART BOOT MODE
  • POWER-ON the EVM
  • You should see character "C" getting printed on the UART terminal every 2-3 seconds as shown below

UART output in UART BOOT MODE
  • Close the UART terminal as shown below. This is important, else the UART script in next step wont be able to connect to the UART port.

Close UART terminal
Note
For HS-FS device, use default_sbl_null_nor_hs_fs.cfg as the cfg file.
  • Open a command prompt and run the below command to flash the SOC initialization binary to the EVM.
      cd ${SDK_INSTALL_PATH}/tools/boot
      python uart_uniflash.py -p COM<x> --cfg=sbl_prebuilt/j722s-evm/default_sbl_null_nor_hs_fs.cfg
    
    • On Linux,
      • The name for UART port is typically something like /dev/ttyUSB0
      • On some Linux systems, one needs to use python3 to invoke python3.x, just python command may invoke python 2.x which will not work with the flashing script.
  • After all the flashing is done, you will see something like below

Parsing config file ...
Parsing config file ... SUCCESS. Found 4 command(s) !!!
Executing command 1 of 4 ...
Found flash writer ... sending sbl_prebuilt/j722s-evm/sbl_uart_uniflash.release.hs_fs.tiimage
Sent flashwriter sbl_prebuilt/j722s-evm/sbl_uart_uniflash.release.hs_fs.tiimage of size 326351 bytes in 32.69s.
Executing command 2 of 4 ...
Command arguments : --operation=flash-phy-tuning-data
Sent flash phy tuning data in 1.65s.
[STATUS] SUCCESS !!!
Executing command 3 of 4 ...
Command arguments : --file=sbl_prebuilt/j722s-evm/sbl_null.release.hs_fs.tiimage --operation=flash --flash-offset=0x0
Sent sbl_prebuilt/j722s-evm/sbl_null.release.hs_fs.tiimage of size 328143 bytes in 33.82s.
[STATUS] SUCCESS !!!
Executing command 4 of 4 ...
Command arguments : --file=../../examples/drivers/sciclient/sciclient_get_version/j722s-evm/wkup-r5fss0-0_freertos/ti-arm-clang/sciclient_get_version.release.appimage.hs_fs --operation=flash --flash-offset=0x80000
Sent ../../examples/drivers/sciclient/sciclient_get_version/j722s-evm/wkup-r5fss0-0_freertos/ti-arm-clang/sciclient_get_version.release.appimage.hs_fs of size 126459 bytes in 14.91s.
[STATUS] SUCCESS !!!
All commands from config file are executed !!!
  • If flashing has failed, see Flash tool error messages and solutions, and resolve the errors.
  • If flashing is successful, do the next steps ...
  • POWER-OFF the EVM
  • Switch the EVM boot mode to OSPI NOR mode as shown below,

OSPI NOR BOOT MODE
  • Re-connect the UART terminal in CCS window as shown in Setup UART Terminal
  • POWER-ON the EVM
  • You should see output like below on the UART terminal
      Starting NULL Bootloader ...
    
      DMSC Firmware Version 9.0.6--w2023.01-j722s (Kool Koa
      DMSC Firmware revision 0x9
      DMSC ABI revision 3.1
    
      INFO: Bootloader_runCpu:162: CPU mcu-r5f is initialized to 800000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU main-r5f0 is initialized to 800000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU c75ss0-01 is initialized to 1000000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU c75ss1-0  is initialized to 1000000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU a530-0 is initialized to 1250000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU a530-1 is initialized to 1250000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU a531-0 is initialized to 1250000000 Hz !!!
      INFO: Bootloader_runCpu:162: CPU a531-1 is initialized to 1250000000 Hz !!!
      INFO: Bootloader_loadSelfCpu:215: CPU wkup-r5f is initialized to 800000000 Hz !!!
      Sciserver Testapp Built On: Mar 19 2024 11:09:15
      Sciserver Version: v2024.03.0.0REL.MCUSDK.09.02.00.17
      RM_PM_HAL Version: w2023.02-j722s
      Starting Sciserver..... PASSED
      SYSFW Firmware Version 9.0.6--w2023.01-j722s (Kool Koa
      Firmware revision 0x9
      ABI revision 3.1
      [SCICLIENT] CPU clock frequency = 800000000 Hz
      All tests have passed!!
    
  • Congratulations now the EVM is setup for loading and running from CCS !!!
  • You dont need to do these steps again unless you have flashed some other binary to the flash.
  • Now you can build a example of interest (see Build a Hello World example) and then run it (see CCS Launch, Load and Run)
Attention
If SBL NULL is used for development, GEL files aren't required for MCU-R5FSS0-0

Additional Details

Note
This section has more details on J722S-EVM. This is mainly for reference and can be skipped unless referred to by other pages in this user guide.

SOC Initialization

Before any program can be loaded and run on the EVM, the SOC needs to be initialized. Refer Flash SOC Initialization Binary section on how to flash SOC initialization binary.

BOOT MODE

UART BOOT MODE

This mode is used to flash files to the board flash via UART. It can also be used to boot applications via UART.

BOOTMODE [ 8 : 15 ] (SW4) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW3) = 1101 1100

UART BOOT MODE

OSPI NOR BOOT MODE

This mode is used to boot flashed applications via EVM flash like OSPI NOR flash

BOOTMODE [ 8 : 15 ] (SW4) = 0100 0000
BOOTMODE [ 0 : 7 ] (SW3) = 1100 1110
BOOTMODE [ 0 : 7 ] (SW2) = 0XXX XXXX

OSPI BOOT MODE

OSPI SERIAL NAND BOOT MODE

This mode is used to boot flashed applications via EVM flash like OSPI Serial NAND flash

BOOTMODE [ 8 : 15 ] (SW4) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW3) = 1100 0000
BOOTMODE [ 0 : 7 ] (SW2) = 1XXX XXXX

OSPI NAND BOOT MODE

SD BOOT MODE

This mode is used to boot applications via SD card on the EVM.

BOOTMODE [ 8 : 15 ] (SW4) = 0100 0000
BOOTMODE [ 0 : 7 ] (SW3) = 1100 0010

SD BOOT MODE

EMMC BOOT MODE

This mode is used to boot applications via eMMC on the EVM.

BOOTMODE [ 8 : 15 ] (SW4) = 0000 0000
BOOTMODE [ 0 : 7 ] (SW3) = 1101 0011

EMMC BOOT MODE

Troubleshooting EVM issues

  • JTAG connection fails on some EVMs with the following error. Need to connect the JTAG cable after board is powered on.

JTAG Connection Error Dialog